2019-03-31 9:46 AM
Hello, all!
I need to explore an option to connect a DRAM to an MCU, and still ahve at least 40 PIOs and 16 AIOs left. and would like your input:
Thanks in advance!
2019-03-31 9:57 AM
How big a DRAM are you talking about ? If not in the gigabits there may be alternatives that are easier to connect.
Alternatively look at the STM32MP1, but not sure if it would have the pins left that you need as I've never looked at it in detail.
2019-03-31 10:06 AM
Hi Mike! Thanks for the quick reply!
The DRAM is 16-Mbit.
2019-03-31 10:20 AM
ok just beyond a serial SRAM or FRAM then, unless you don't mind using four of them. Best bet is probably the MP1 or any other Cortex-A processor then which can address gigabytes.
Alternative is to build a DRAM controller with an FPGA,
2019-03-31 10:21 AM
Thinking more, how busy is your MCU ? You could implement the DRAM refresh using a timer interrupt.
2019-03-31 10:35 AM
I better present the problem properly:
I need to connect a vga camera for taking pictures, which are stored and later sent to a remote server.
I have an SPI flash memory.
I need to be sure that I can save images to the flash memory fast enough before I get the camera buffer overrun (the camera itself is not chosen yet, I need to be prepared).
The image will be up to 640*480 = 308KB.
One solution is having an MCU with a large enough RAM, but those are expensive, going 7+ USD.
Another solution is having a DRAM, saving everything into it, and then reading out of it into the flash, once the image finished transferring.
If the 16Mbit DRAM is problematic, I suppose I can go as low as 4Mbit (which is 512Kbit, which should fit the image)
2019-03-31 11:08 AM
If it's going into an out of the flash, why not just use a faster flash.
But aren't you going to wear it out quite quickly ?
2019-03-31 12:25 PM
The flash is not a problem - the system only snaps 2 pictures a day, the flash is 8MB and has 100K write cycles.
The only problem is reading the data fats enough.
After further discussion, I understand that DRAM is too unstable for us, so I suppose I'm down to SRAM or a large enough RAM (or maybe another option I'm not seeing?)
2019-03-31 6:45 PM
What STM32?
Check the STM32F429I or STM32F469 DISCO board schematic showing SDRAM implementation. Review relevant Reference Manuals.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.