2024-11-11 3:20 AM - last edited on 2024-11-11 3:37 AM by mƎALLEm
Hi
I am trying to send some CAN-bus messages from a STM32H723VGT6 mounted on a BIGTREETECH SKR 3 EZ V1.0
I am following this video to send standard CAN messages in external loopback mode (https://www.youtube.com/watch?v=kXyzaaSk6Qs&t=568s&ab_channel=ControllersTech). But whenever I reach the point where I add a message to the TxFifo I get the error 0x20 -> "Parameters error" but I am not sure what could be causing this
Here are the parameters I set for FDCAN1
To avoid additional variables we used the internal clock of the microprocessor, here is the final frequency of the FDcan peripheral
And the transreceiver mounted on the board is the mcp2542fd-e/sn
Solved! Go to Solution.
2024-11-11 6:11 AM
Hello,
As your first issue has been solved please accept as solution the comment that answered your question and open a new thread.
Thank you for your understanding.
2024-11-11 6:40 AM
Ok, thank you for all the help
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.