2020-12-16 6:26 AM
Hello !
I'm trying to communicate with a ADC : AD7276. With my MCU STM32H745
To get the values from the ADC, I set the CS in low state and CLK 16 times.
However, the HAL_SPI_Receive_DMA method does not activate the clock on the SPI.
What are the parameters to activate the clock with this method?
I tried with the HAL_SPI_TransmitReceive_DMA method. But the first byte is missing ( while the byte in TX is transmited ).
I am in fullduplex and DMA TX/RX 8-ByteDataSize.
Thanks You :)
Solved! Go to Solution.
2020-12-16 6:39 AM
2020-12-16 6:39 AM
Oups !! Nothing ^^
It's work in RX mode :3
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.