cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G0B1 FDCAN Reset

Nabidev
Associate II

Hello,

 

in an earlier post it was suggested to reset the FDCAN for full error recovery using RCC_APBRSTR1.FDCANRST Bit

This bit seems to be global for all FDCAN instances.

Is it correct that full error recovery in one FDCAN instance is not possible without interrupting traffic in the other instance - as all (or both in case of stm32g0b1) instances have to be reset?

 

t

1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello,

Do you mean a recovery from Bus-Off state?

This is How to recover from Bus-Off state with FDCAN on STM32 MCUs without performing a reset of the peripheral.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
mƎALLEm
ST Employee

Hello,

Do you mean a recovery from Bus-Off state?

This is How to recover from Bus-Off state with FDCAN on STM32 MCUs without performing a reset of the peripheral.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.