2020-11-21 8:04 AM
I've read in RM that, when running on 64 MHz it has 2 wait states, meaning that 1 cycle instructions execution takes actually 3 cycles. If I understand this correctly, that means that the effective speed is actually 21.3 MHz? What use is there using 64 MHz then? Or there is parallel pipelines for instruction execution? What is then effective speed, if there are two pipelines?
Solved! Go to Solution.
2020-11-21 9:20 AM
Dear @Siniša Marović
That is a nice question ! I Invite you to jump to our On-line Training here - your can go to Slide 13 directly where we explain how our Flash and Flash accelerators are working to get the best performance with the core running at 64MHz :
https://st-onlinetraining.s3.amazonaws.com/STM32G0-Memory-Flash-%28FLASH%29/index.html
and also the Cortex-M0+ Introduction and Pipeline with the instruction set
https://st-onlinetraining.s3.amazonaws.com/STM32G0-System-ARM_Cortex_G0-%28Core%29/index.html
Cheers,
STOne-32.
2020-11-21 9:20 AM
Dear @Siniša Marović
That is a nice question ! I Invite you to jump to our On-line Training here - your can go to Slide 13 directly where we explain how our Flash and Flash accelerators are working to get the best performance with the core running at 64MHz :
https://st-onlinetraining.s3.amazonaws.com/STM32G0-Memory-Flash-%28FLASH%29/index.html
and also the Cortex-M0+ Introduction and Pipeline with the instruction set
https://st-onlinetraining.s3.amazonaws.com/STM32G0-System-ARM_Cortex_G0-%28Core%29/index.html
Cheers,
STOne-32.
2020-11-21 12:08 PM
Yes, that's what I needed. So, if I understand correctly, for linear code block with prefetch and instruction cache on, simple load/store instructions should be executed at speed of 1 instruction per cycle. Even to ports?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.