STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F4 discovery - DMA2 TC interrupt does not triggered

Hi, guys.Here is short description of my project:I have an ADC, that samples data via one regular channel and result sended via DMA. This DMA are working in Normal mode, so after DMA compete its transmission I processed received data and then enable ...

chupys by Associate II
  • 2888 Views
  • 4 replies
  • 0 kudos

Troubleshooting ADC2 on STM32L412KB

Hi,I'm using both ADC's on the STM32L412KB, code is generated used the STM32 Cude with Low Level Drivers.ADC1 works as expected, but ADC2 always reads 0, no matter in which configuration. So I'm assuming it's not a hardware fault, but a configuration...

0693W000005CBx3QAG.png
CLang.3 by Associate
  • 928 Views
  • 0 replies
  • 0 kudos

Resolved! STM32L476RG Differential ADC functioning as singled-ended

I am working on a project using the STM32L476RG microcontroller and have run into an issue with using the ADC in differential configuration. When using the ADC configured as differential the output from the ADC is the same as if it was configured as ...

0693W000005C3QuQAK.png
Kcloc.1 by Associate II
  • 9762 Views
  • 6 replies
  • 1 kudos

Resolved! STM32L4R5ZI stucked on polling for adc conversion

Hi, I'm using STM32L4R5ZI nucleo board for my thesis project. But I have a problem doing a very easy thing: read an ADC conversion value. The program do just this: read the value and sends it over usart. The program does this:HAL_ADCEx_Calibration_St...

0693W000005C9fvQAC.jpg

STM32F072C8 Reliability Information for ISO26262 ASIL

I dont want to use the MIL HBK 217 to calculate the MTBF/FIT rate because it will be dreadfully low. Could you please provide the reliability(MTBF/FIT) information for the STM32F072C8 micro? Thank you I need this for an ASIL project that we are wo...

MBrem.2 by Associate
  • 851 Views
  • 0 replies
  • 0 kudos

SD card class

Hi everybody,With a 4 bits SDIO and stm32f446RE i can read and write data from SD using the FatFs lib, no problem. Ths Sd card is a sanDisk Ultra 8GB (10) MicroSd HC1 class1461. using 512bytes transfers (sector size), the write speed is not so amazin...

papageno by Associate III
  • 1184 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.