cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G030F6 uart dma idle interrut CNDTR not work properly

XWang.4
Associate

Hi, team,

I am work on stm32g030f6's uart dma. And config them as idle interrut mode to receive data.

When the uart data on high frequence like 10bytes/30ms , the CNDTR will be aways MY_BUFF_LEN -1 , so i only can receive 1 byte data. After reset the power it will be ok, i already test the code on stm32f103 and worked properly. But not good on stm32g030 !!! Help guys! i think stm32g030 has bug on dma CNDTR register

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
TDK
Super User

If CNDTR = MY_BUFF_LEN - 1, it means the DMA can receive that many more bytes before stopping.

If CNDTR is frozen at that value, despite signals being sent, it could be because the DMA had an error and stopped itself. Examine the DMA->ISR register to investigate.

If you feel a post has answered your question, please click "Accept as Solution".
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.