STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ADC to DAC problem

Hi guys, I have a problem with ADC conversion I would say. I put sine wave on ADC input and then I just transfer the value to DAC register, but the negative half of the sine wave is clipped. The code is just this ( Inside HAL_ADC_ConvCpltCallback):DA...

0693W000006HJO0QAO.jpg 0693W000006HJNvQAO.jpg
binarybee by Associate III
  • 1171 Views
  • 1 replies
  • 0 kudos

There seems to be a difference between the system clock immediately after the firmware update and the system clock after the reset (or after power off->on).

Hello. I am using stm32f765 series mcu with iar compiler. A strange thing was caught during development and I left an inquiry.The problem I'm facing seems to be the difference between the system clock right after the firmware is uploaded and the syst...

YKim.5 by Associate
  • 1728 Views
  • 2 replies
  • 0 kudos

Resolved! SPI not working with MISO connected to 3V and 0V

I am trying to code SPI functionality to connect with an external 16-bit ADC. The STM32 only receives data from the ADC, so only a MISO and SCLK line, along with a Conversion/CS line is required. I am currently using the 32F072BDISCOVERY board to te...

JAlle.2 by Associate II
  • 5831 Views
  • 11 replies
  • 0 kudos

STM32G030F6 uart dma idle interrut CNDTR not work properly

Hi, team, I am work on stm32g030f6's uart dma. And config them as idle interrut mode to receive data.When the uart data on high frequence like 10bytes/30ms , the CNDTR will be aways MY_BUFF_LEN -1 , so i only can receive 1 byte data. After reset the ...

XWang.4 by Associate
  • 1746 Views
  • 1 replies
  • 0 kudos

Need a counter to count in micro seconds

Hi All,I am using STM32F74xxx.I need to count micro seconds. currently we are using HAL_GetTick(), function but it gives the time in ms.After I searched on google I found some ways to get micro seconds count, and I tried it but no luck.can any one he...

RRajb.1 by Associate II
  • 3406 Views
  • 4 replies
  • 0 kudos

Can't update GPIOx_MODER register value in STM32H753.

I work with STM32H753 through 3-rd side hardware (Algocraft WN-1 programmer) and have an access to the registers. I try to read/write GPIOJ pins. For this purpose I enabled GPIOJ clock by writing the AHB4 peripheral clock enable register (RCC_AHB4ENR...

LKuri.1 by Associate II
  • 1009 Views
  • 2 replies
  • 0 kudos

2021 STM32 Wish List

Dear Community Members & STM32 fans,Peculiar year it has been, 2020 comes to its end. This is an opportunity to say "Thank you" because:you don't hesitate to bring help to othersyou help us improve our STM32 offeryou have confidence on ST Communityyo...

Resolved! AXI SRAM losing last few writes across reset

it seems that a write to AXI SRAM very shortly before a system reset (via AIRCR) gets lost. I wrote a very short block of code that simply reads a word from 0x24000000, increments it, writes it back, and resets the processor. I can see that the value...

CHead by Associate III
  • 8036 Views
  • 12 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.