2017-12-11 5:58 AM
Hi everyone,
I am using STM32F769I Eval Board and i am trying to run the STM32Cube_FW_F7_V1.7.0 CAN_Networking example.
First i read the documentation and set the jumpers
+-------------+-----------------+
| Jumper | CAN1 |
+-------------+-----------------+
| JP14 | fitted |
| JP19 | 1-2 |
| JP18 | fitted |
+-------------+-----------------+
Then, i connected to device and try to set the bit rate 250 000 Kbit/s which is 1Mbit/s but i could not figure it out how.
And i am suspicious that this examples work properly, is there anyone having issues with that or anyone can set the bit rate to 250 000 Kbit/s?
By the way, i am new to this
Thans in advance,
#can-bus #can-bus-bit-timing #stm32f7-evalWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.