2018-05-29 11:34 PM
Hello friends,
I try SPI communication, and I have a problem. I only send data.... But how to receive it?
Connection is:
1. one master - one slave
2. Full duplex
Initialize:
LL_SPI_InitTypeDef SPI_InitStruct;
LL_GPIO_InitTypeDef GPIO_InitStruct;LL_SPI_Disable(SPI1);
LL_AHB1_GRP1_EnableClockLL_AHB1_GRP1_PERIPH_GPIOA);
LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_SPI1);
/* SPI2 GPIO Configuration */
GPIO_InitStruct.Pin = LL_GPIO_PIN_5; GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE; GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_VERY_HIGH; GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL; GPIO_InitStruct.Pull = LL_GPIO_PULL_NO; GPIO_InitStruct.Alternate = LL_GPIO_AF_5; LL_GPIO_Init(GPIOA, &GPIO_InitStruct); GPIO_InitStruct.Pin = LL_GPIO_PIN_7; GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE; GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_VERY_HIGH; GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL; GPIO_InitStruct.Pull = LL_GPIO_PULL_NO; GPIO_InitStruct.Alternate = LL_GPIO_AF_5; LL_GPIO_Init(GPIOA, &GPIO_InitStruct); GPIO_InitStruct.Pin = LL_GPIO_PIN_6; GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE; GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_VERY_HIGH; GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL; GPIO_InitStruct.Pull = LL_GPIO_PULL_NO; GPIO_InitStruct.Alternate = LL_GPIO_AF_5; LL_GPIO_Init(GPIOA, &GPIO_InitStruct); GPIO_InitStruct.Pin = LL_GPIO_PIN_4; GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE; GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_VERY_HIGH; GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL; GPIO_InitStruct.Pull = LL_GPIO_PULL_NO; GPIO_InitStruct.Alternate = LL_GPIO_AF_5; LL_GPIO_Init(GPIOA, &GPIO_InitStruct);/* SPI1 parameter configuration*/
SPI_InitStruct.TransferDirection = LL_SPI_FULL_DUPLEX; SPI_InitStruct.Mode = LL_SPI_MODE_MASTER; SPI_InitStruct.DataWidth = LL_SPI_DATAWIDTH_8BIT; SPI_InitStruct.ClockPolarity = LL_SPI_POLARITY_HIGH; SPI_InitStruct.ClockPhase = LL_SPI_PHASE_1EDGE; SPI_InitStruct.NSS = LL_SPI_NSS_HARD_OUTPUT; SPI_InitStruct.BaudRate = LL_SPI_BAUDRATEPRESCALER_DIV64; SPI_InitStruct.BitOrder = LL_SPI_MSB_FIRST; SPI_InitStruct.CRCCalculation = LL_SPI_CRCCALCULATION_DISABLE; SPI_InitStruct.CRCPoly = 7; LL_SPI_Init(SPI1, &SPI_InitStruct);LL_SPI_SetStandard(SPI1, LL_SPI_PROTOCOL_MOTOROLA);
LL_SPI_EnableNSSPulseMgt(SPI1);LL_SPI_SetRxFIFOThreshold(SPI1, LL_SPI_RX_FIFO_TH_QUARTER);
/* Configure SPI1 transfer interrupts */
/* Enable RXNE Interrupt */ LL_SPI_EnableIT_RXNE(SPI1);LL_SPI_Enable(SPI1);
And function to write/read....
int32_t read_from_reg(SPI_TypeDef *SPI, uint8_t data, uint8_t *SPI_Data_receive)
{ LL_SPI_TransmitData8(SPI, data); while (!LL_SPI_IsActiveFlag_TXE(SPI)); while (!LL_SPI_IsActiveFlag_RXNE(SPI)); while (LL_SPI_IsActiveFlag_BSY(SPI)); *SPI_Data_receive = LL_SPI_ReceiveData8(SPI);return 0;
}And I sent one byte and I don't receive anything. Any idea, how to receive some data from register?
#nucleo-f767zi #stm32f7-spi Note: this post was migrated and contained many threaded conversations, some content may be missing.2018-08-11 11:39 PM
Hey. If it has 4 words fifo, how can i send only one or two data packets ? :(
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.