2015-07-07 11:13 AM
I've seen at least two other threads with an inverted DAC concern being present, wondering if anyone has more information o the issue? I have 3 identical boards in house populated with the F4, one of which has an inverted DAC output.
I'm not finding any errata on this, only seeing others experiencing a similar issue.All three boards are running identical code. All boards seem to work properly in GPIO mode. My sample size on this issue is small, but if this is a possible concern to any magnitude I would like to identify it before it is too late in the development process. Any input that may be out there would be very helpful. #dac-inverted-stm32f42015-07-07 11:31 AM
Seen a couple of reports, but I'm not sure if it's not a board, soldering or ESD issue.
2015-07-07 11:57 AM
Thanks for the reply Clive.
I contacted ST directly as well, hopefully someone has an understanding of the fault mechanism so it can be prepared for/avoided on our end. We are pretty careful about design and build here, so I'm cautiously optimistic it isn't a goof on our end. The ESD item is my biggest fear. If the DAC has the possibility to permanently invert from a static hit...that is going to be a bit of a problem in the planned use.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.