STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F427 Inverted DAC output

Posted on July 07, 2015 at 20:13I've seen at least two other threads with an inverted DAC concern being present, wondering if anyone has more information o the issue? I have 3 identical boards in house populated with the F4, one of which has an inve...

STM32F407VET PLL problem

Posted on July 07, 2015 at 17:00 I used STM32 cube for the PLL configuration // Enable HSE Oscillator and activate PLL with HSE as source RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE; RCC_OscInitStruct.HSEState = RCC_HSE_...

kareemkna by Associate II
  • 3770 Views
  • 11 replies
  • 0 kudos

4 channel frequency measurement on a single timer

Posted on July 07, 2015 at 18:18I've been testing a STM32F4 Discovery since I'm new to ST Microcontrollers and I wanted to use one timer to measure 4 different channel frequencies, as I want to measure more signals than there are timers. I do not ca...

0690X00000605XPQAY.png 0690X00000605JSQAY.png 0690X00000605XeQAI.png
jackygip by Associate II
  • 1784 Views
  • 2 replies
  • 0 kudos

Optimization in CooCox on an STM32F415VG

Posted on July 07, 2015 at 11:49Hi guys, I have code that has been working great for a couple of months now on an STM32F415VG, but I added some libaries/code yesterday which took it beyond the flash sectors that I wanted it to sit in (it's a custom ...

Timer Interrupt for UART communication

Posted on July 07, 2015 at 09:47 Hello, I want STM32 with GSM board each sec communicate. in Main.c int main(void) { HAL_Init (); SystemClock_Config (); HARD_LED_Init(LED_GREEN); Term_UART_Config(); HARD_TIM_Init(); while (1) ...

astree by Associate II
  • 2295 Views
  • 4 replies
  • 0 kudos

Sharing functions between two pieces of code

Posted on July 07, 2015 at 16:27My subject doesn't quite describe what I'm trying to do, but not quite sure how else to explain: I have a bootloader stored at the start of flash in my STM32f415 (flash location 0x08000000), and my main application is...

usart dma - receive

Posted on July 06, 2015 at 13:36hej, can anyone tell me why dma is  not working?...but the usart works...volatile uint8_t Buffer[32];uint8_t receiveword;/**************************************************************************************/void gpi...

arunl4g by Associate II
  • 2566 Views
  • 8 replies
  • 0 kudos

STM32F4 discovery RTC problem

Posted on July 07, 2015 at 10:32The original post was too long to process during our migration. Please click on the attachment to read the original post.

matas by Associate II
  • 1319 Views
  • 2 replies
  • 0 kudos

Keil and stm32CubeMX generated USB CDC project

Posted on February 13, 2015 at 17:40I generated a USB CDC driver using Cube MX for the STM32L0538 DISCO. This compiled and linked and connected to a PC.I tried to send some bytes using CDC_Transmit() but I then get USB NOT RECOGNIZED.Seems to be a h...

Stm32User by Associate III
  • 2469 Views
  • 6 replies
  • 0 kudos

Position independent code for STM32F4

Posted on July 06, 2015 at 04:18MCU: STM32F4 (ARM Cortex M4) Build environment: arm-none-eabi-gcc 4.8.4 20140725 My goal is to build an image that can be run from any properly-aligned offset in internal flash. My ideal scenario is for the code would...

squeamz by Associate
  • 2139 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.