2018-08-23 6:20 AM
Everything works fine when the USB programming port is connected to PC.
When the board is supplied from external +5V then the reset signal is
active all the time. The reset disappears when I connect USB programming
port. It seams that the STM32F103C8T6 forces low the line T_NRST until
it gets USB connection.
Is this an expected behavior? What can I do to use the board without USB?
There is a solder bridge SB11 which connects T_NRST to the NRST of the
main processor and I could remove it. But then I probably could not be
able to upload new software through USB.
2018-08-23 6:28 AM
Update the firmware in the STLink (STM32F103).
JW
2018-08-23 6:32 AM
OK JW, how to do it? I am using Atollic TrueSTUDIO for STM32 ver.9.0.0.
2018-08-23 6:42 AM
Done! I have found - Help / Tools / ST-Link Upgrade.
It is fine after the update .
Thank you JW.
Grzesiek
2018-08-23 6:57 AM
The V24 or V25 shipped on the STM32f407G-DISC1 would hold the target in reset.
Most current is V31 which is available as a stand-alone upgrade
https://www.st.com/en/development-tools/stsw-link007.html
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.