2014-07-08 8:39 AM
Hi everybody!
I want to migrate from STM32F407 to STM32F427, and use the full power of this microprocessor (180MHz instead of 168MHz), because I need more speed ressources.First, I find this new application note:http://www.st.com/web/en/resource/technical/document/application_note/DM00123028.pdfDo you know what is the frequency overdrive mode ?Secondly, I want to set the new maximum frequency on my project (I already use a STM32F427 but at lower frequency). I use an external oscillator of 8MHz.I use this clock parameters for the moment:SystemCoreClock = 168000000;
PLL_M = 8
PLL_N = 336
PLL_P = 2
PLL_Q = 7
AHBPrescTable[16] = {0, 0, 0, 0, 0, 0, 0, 0, 1, 2, 3, 4, 6, 7, 8, 9};
HSE_VALUE = 8000000
Can I only change the parameter
SystemCoreClock
to180000000
? Because it works but I don't know if the speed of core change.
Thank you very much!2014-08-19 4:20 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.