STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USART Buffer: How can I set priorities?

Posted on August 19, 2014 at 18:04 Hello everybody! I coded a buffer for my USART output. This is how it looks like: #define FIFO_BUFFER_SIZE 64 #define BUFFER_MASK (FIFO_BUFFER_SIZE-1) typedef struct FifoStruct { volatile uin...

jean by Senior
  • 1158 Views
  • 2 replies
  • 0 kudos

TIMER WITH EXTERNAL CLOCK PIN STM32F429

Posted on August 20, 2014 at 14:14Hi!!!I would like to connect the GPIO A6 to the timer 13 as input capture and also to the timer 3 as external clock. I've tried to use the input connected only to timer 13 and it runs ( it reaches the interrupt rout...

gerson74 by Associate II
  • 1345 Views
  • 1 replies
  • 0 kudos

STM32L152RE documentation and capture timer problem

Posted on August 19, 2014 at 19:55Hi,I am new with programming STM32 but I've experience with MSP430. I'm looking for information on setting timer / capture timer. TI has many user guide and complete datasheet explaining each register. I didn't find...

How to determine output compare channels number

Posted on August 20, 2014 at 10:23Hello, First of all, I want to determine how many output compare channel  the STM32F407VGT6 (STM32F4DISCO'S MCU) has. In the PIC32 MCU's for example, Output Compares are regarded as separate devices even if they nee...

LCD_DisplayStringLine(Line5, ''Hello'');

Posted on August 18, 2014 at 15:44Where can I find the definition of LINE(5)? I would appreciate for it. Jai Please note that: &sharpdefine Line5 LCD_LINE_5  at stm32_eval.h &sharpdefine LCD_LINE_5 LINE(5) at stm3210c_eval_lcd.h #lmgtfy #stm32f10...

jeu by Associate II
  • 1906 Views
  • 5 replies
  • 0 kudos

STM32F4 Hardware Flow Control

Posted on August 20, 2014 at 04:39I am communicating with an STM32F407 from a computer via Serial. I would like to implement flow control, but I have some questions.1) Can I manually control the RTS line, so that I can receive a command from the PC ...

Problem with SPI2 on STM32F103RB

Posted on August 20, 2014 at 03:11Hello, I want to use SPI2 on STM32F103RB to communicate with RFM12 module but SPI does not work. Can you help me where is a problem?This is the definitions:#define RFM_SPI2_PORT GPIOB#define RFM_GPIO_CLK           ...

0690X000006056iQAA.png

STM32F407 > STM32F427 MIGRATION

Posted on July 08, 2014 at 17:39Hi everybody!I want to migrate from STM32F407 to STM32F427, and use the full power of this microprocessor (180MHz instead of 168MHz), because I need more speed ressources.First, I find this new application note:http:/...

PLL Config Reg Not Changing w/ RCC_PLLConfig

Posted on August 19, 2014 at 21:41 Having a strange problem; not sure if it's an anomaly of my compiler (IAR) or I'm doing something wrong: I'm trying to change SYSCLK for the STM32F427, which uses the PLL as the SYSCLK source. The issue ...

jvavra by Associate III
  • 1265 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.