2015-03-13 4:33 AM
Hi! I modified the following program to get a pulse of 5V and 40kHz of frequency. I tried it in an oscilloscope and I get a 4V pulse and 12,8kHz frequency. What is wrong in the code??
#include ''stm32f4xx.h''
#include ''stm32f4xx_rcc.h''
#include ''stm32f4xx_gpio.h''
#include ''stm32f4xx_tim.h''
void TM_LEDS_Init(void) {
GPIO_InitTypeDef GPIO_InitStruct;
/* Clock for GPIOA */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);
*/
/* Alternating functions for pins */
GPIO_PinAFConfig(GPIOA, GPIO_PinSource6, GPIO_AF_TIM13);
/* Set pins */
GPIO_InitStruct.GPIO_Pin = GPIO_Pin_6;
GPIO_InitStruct.GPIO_OType = GPIO_OType_OD;
GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStruct.GPIO_Speed = GPIO_Speed_100MHz;
GPIO_Init(GPIOA, &GPIO_InitStruct);
}
void TM_TIMER_Init(void) {
TIM_TimeBaseInitTypeDef TIM_BaseStruct;
/* Enable clock for TIM13 */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM13, ENABLE);
/*
Set timer prescaler
Timer count frequency is set with
timer_tick_frequency = Timer_default_frequency / (prescaller_set + 1)
In our case, we want a max frequency for timer, so we set prescaller to 0
And our timer will have tick frequency
timer_tick_frequency = 84000000 / (0 + 1) = 84000000
*/
TIM_BaseStruct.TIM_Prescaler = 0;
/* Count up */
TIM_BaseStruct.TIM_CounterMode = TIM_CounterMode_Up;
/*
Set timer period when it have reset
First you have to know max value for timer
In our case it is 16bit = 65535
To get your frequency for PWM, equation is simple
PWM_frequency = timer_tick_frequency / (TIM_Period + 1)
If you know your PWM frequency you want to have timer period set correct
TIM_Period = timer_tick_frequency / PWM_frequency - 1
In our case, for 40Khz PWM_frequency, set Period to
TIM_Period = 84000000 / 40000 - 1 = 2099
If you get TIM_Period larger than max timer value (in our case 65535),
you have to choose larger prescaler and slow down timer tick frequency
*/
TIM_BaseStruct.TIM_Period = 2099; /* 10kHz PWM */
TIM_BaseStruct.TIM_ClockDivision = TIM_CKD_DIV1;
TIM_BaseStruct.TIM_RepetitionCounter = 0;
/* Initialize TIM13 */
TIM_TimeBaseInit(TIM13, &TIM_BaseStruct);
/* Start count on TIM13 */
TIM_Cmd(TIM13, ENABLE);
}
void TM_PWM_Init(void) {
TIM_OCInitTypeDef TIM_OCStruct;
/* Common settings */
/* PWM mode 2 = Clear on compare match */
/* PWM mode 1 = Set on compare match */
TIM_OCStruct.TIM_OCMode = TIM_OCMode_PWM2;
TIM_OCStruct.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCStruct.TIM_OCPolarity = TIM_OCPolarity_Low;
/*
To get proper duty cycle, you have simple equation
pulse_length = ((TIM_Period + 1) * DutyCycle) / 100 - 1
where DutyCycle is in percent, between 0 and 100%
50% duty cycle: pulse_length = ((2099 + 1) * 50) / 100 - 1 = 1049
Remember: if pulse_length is larger than TIM_Period, you will have output HIGH all the time
*/
TIM_OCStruct.TIM_Pulse = 1049; /* 50% duty cycle */
TIM_OC1Init(TIM13, &TIM_OCStruct);
TIM_OC1PreloadConfig(TIM13, TIM_OCPreload_Enable);
}
int main(void) {
/* Initialize system */
SystemInit();
/* Init leds */
TM_LEDS_Init();
/* Init timer */
TM_TIMER_Init();
/* Init PWM */
TM_PWM_Init();
while (1) {
}
} Thank you
#stm32f407 #stm32f4 #discovery #timers
2015-03-13 5:32 AM
12.8 KHz because you haven't set the HSE_VALUE and PLL settings correctly for your board. Looks to be assuming you have a 25 MHz source, but you really have an 8 MHz one.
4V would probably do with loading, and how aggressively you're pulling up the output. Think potential divider.2015-03-20 3:45 AM
So how do I have to configure the HSE_VALUE and PLL settings?
Thank you for response2015-03-20 5:26 AM
HSE_VALUE is often defined in stm32f4xx_conf.h for the project, and the PLL settings in system_stm32f4xx.c
For examples of these files/settings review the examples in thehttp://www.st.com/web/en/catalog/tools/PF257904
. The red download button at the bottom....
/* Define to prevent recursive inclusion -------------------------------------*/
#ifndef __STM32F4xx_CONF_H
#define __STM32F4xx_CONF_H
#if defined (HSE_VALUE)
/* Redefine the HSE value; it's equal to 8 MHz on the STM32F4-DISCOVERY Kit */
#undef HSE_VALUE
#define HSE_VALUE ((uint32_t)8000000)
#endif /* HSE_VALUE */
...
/* PLL_VCO = (HSE_VALUE or HSI_VALUE / PLL_M) * PLL_N */
#define PLL_M 8
#define PLL_N 336
2015-03-20 6:10 AM
Thank you very much! I made it.
2015-03-23 7:54 AM
Hi Clive, one more question. Now that I have a timer making a pulse indefinitely I would like to configure another timer that control the first timer. The idea is that the new timer let me to do for example, pulses for 1 sec and then stop for 10 sec and then again pulses for 1 sec.....
Can you help me please? Thanky you very much2015-03-23 9:35 AM
Quick blind example, using a single timer, with modulating output.
// STM32F4-Discovery TIM13 40KHz PWM, modulating 1 second ON, 10 seconds OFF (PA.06 TIM13_CH1) - sourcer32@gmail.com &sharpinclude ''stm32f4_discovery.h'' /**************************************************************************/ void RCC_Configure(void) { /* GPIOA clock enable */ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE); /* TIM13 clock enable */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM13, ENABLE); } /**************************************************************************/ void NVIC_Configure(void) { NVIC_InitTypeDef NVIC_InitStructure; /* Enable the TIM13 global Interrupt */ NVIC_InitStructure.NVIC_IRQChannel = TIM8_UP_TIM13_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); } /**************************************************************************/ void GPIO_Configure(void) { GPIO_InitTypeDef GPIO_InitStructure; /* GPIOA Configuration: TIM13 CH1 (PA6) */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP ; GPIO_Init(GPIOA, &GPIO_InitStructure); /* Connect TIM13 pins to AF */ GPIO_PinAFConfig(GPIOA, GPIO_PinSource6, GPIO_AF_TIM13); } /**************************************************************************/ uint32_t Period; void TIM13_Configure(void) { TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; TIM_OCInitTypeDef TIM_OCInitStructure; Period = (SystemCoreClock / 2) / 40000; // 40 KHz, from APB1 clock *2, nominally 84 MHz /* Time base configuration */ TIM_TimeBaseStructure.TIM_Prescaler = 0; TIM_TimeBaseStructure.TIM_Period = Period - 1; TIM_TimeBaseStructure.TIM_ClockDivision = 0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM13, &TIM_TimeBaseStructure); /* PWM1 Mode configuration: Channel1 */ TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1; TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_Pulse = Period / 2; // 50/50 duty TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High; TIM_OC1Init(TIM13, &TIM_OCInitStructure); TIM_OC1PreloadConfig(TIM13, TIM_OCPreload_Enable); /* TIM Interrupts enable */ TIM_ITConfig(TIM13, TIM_IT_Update, ENABLE); /* TIM enable counter */ TIM_Cmd(TIM13, ENABLE); } /**************************************************************************/ void TIM8_UP_TIM13_IRQHandler(void) // 40KHz { static int modulatingcount = 0; // 1 Second On - 40000 ticks // 10 Seconds Off - 400000 ticks // full cycle 440000 ticks if (TIM_GetITStatus(TIM13, TIM_IT_Update) != RESET) // Validate source { TIM_ClearITPendingBit(TIM13, TIM_IT_Update); // Clear source modulatingcount = (modulatingcount + 1) % 440000; if (modulatingcount > 40000) TIM13->CCR1 = 0; // Off else TIM13->CCR1 = Period / 2; // 50/50 duty } } /**************************************************************************/ int main(void) { RCC_Configure(); NVIC_Configure(); GPIO_Configure(); TIM13_Configure(); while(1); // Do not exit } /**************************************************************************/ &sharpifdef USE_FULL_ASSERT /** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @param file: pointer to the source file name * @param line: assert_param error line source number * @retval None */ void assert_failed(uint8_t* file, uint32_t line) { /* User can add his own implementation to report the file name and line number, ex: printf(''Wrong parameters value: file %s on line %d\r\n'', file, line) */ while (1) {} } &sharpendif /**************************************************************************/
2015-04-13 10:42 AM
That looks good! But actually the pulses need to be very precise. I'm using this to create an ultrasonic sensor and calculate some distances, so I should configure the ''hardware'' not ''software'' (code). I read in some posts that maybe the solution is the slave mode, buy I don't know how that works.
Thank you very muchWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.