2015-04-13 8:04 AM
Hello st!
Today i bumped into a problem with code generation for encoders in CubeMx tool. I've read all topics on this site connected to timers in encoder modes, but all i've found was only not-working-code, or almost-working-code. Problem: I would like to run my timers in encoder mode. In other threads i saw Init functions, containing:(...)
encoder.EncoderMode = TIM_ENCODERMODE_TI12;
(...)
HAL_TIM_Encoder_Init(&timer, &encoder);
(...)
Okay, but isn't it something I should be able to choose in Cube, and then this code would have been generated automatically?
If there is no way to configure it via Cube, do i have to write the init functions myself? (Because for that mode timer needs to be initialized via hal_tim_encoder_init function, doesn't it?)
I got a bit confused with this.
Btw. I use F3Discovery
Thank you for your answers!
#stm32 #encoder #tim
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.