2018-05-28 12:05 AM
Im trying to catch data from the unknown device, this device has data and clock. I decided to make my stm32 as spi slave and catch the data as recevier.And im struggling with it. I have this data flow which i want to catch:
Clock is yellow and green is data.
I need only 16bytes from it, when data line goes low, we can see this 16bytes:
And there is the speed of the clock, as you can see its around 1.5us each clock pulse. So what i have to do is configure spi with HAL, i toolk SPI1(PA5 - CLOCK, PA7- DATA) cuz it has more powerful MHZ, chose spi mode ''RECEIVE ONLY SLAVE'', HARDWARE NSS SIGNAL: DISABLED. And here is my spi1 config:
static void MX_SPI1_Init(void)
{/* SPI1 parameter configuration*/
hspi1.Instance = SPI1; hspi1.Init.Mode = SPI_MODE_SLAVE; hspi1.Init.Direction = SPI_DIRECTION_2LINES_RXONLY; hspi1.Init.DataSize = SPI_DATASIZE_8BIT; hspi1.Init.CLKPolarity = SPI_POLARITY_HIGH; hspi1.Init.CLKPhase = SPI_PHASE_1EDGE; hspi1.Init.NSS = SPI_NSS_SOFT; hspi1.Init.FirstBit = SPI_FIRSTBIT_LSB; hspi1.Init.TIMode = SPI_TIMODE_DISABLE; hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE; hspi1.Init.CRCPolynomial = 10; if (HAL_SPI_Init(&hspi1) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }}
What im doing in main.c, as oscilo's pictures says we need to catch the moment when data goes low and then try to read a data, im trying to catch first pulse then wait until data goes high then low and only they read spi, at least only first byte - it should be 0.
int main(void)
{ /* USER CODE BEGIN 1 */ /* USER CODE END 1 *//* MCU Configuration----------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init(); MX_DMA_Init(); MX_USB_DEVICE_Init(); MX_SPI1_Init(); /* USER CODE BEGIN 2 *//* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */ uint8_t collect_bits = 0; char string_array[21] = {0}; uint8_t spi_buffer[16] ={0} ; spi_buffer[0] = 5; // while (1) // { // HAL_Delay(10000); while (HAL_GPIO_ReadPin (GPIOA,GPIO_PIN_7) == 0){} // wait until GPIOC 9 goes high while (HAL_GPIO_ReadPin (GPIOA,GPIO_PIN_7) == 1){} // wait until GPIOC 9 goes high while (HAL_GPIO_ReadPin (GPIOA,GPIO_PIN_7) == 0){} // wait until GPIOC 9 goes high while (HAL_GPIO_ReadPin (GPIOA,GPIO_PIN_7) == 1){} // wait until GPIOC 9 goes high HAL_SPI_Receive(&hspi1, (uint8_t*)spi_buffer, 16,0); /* USER CODE END WHILE *//* USER CODE BEGIN 3 */
// }
/* USER CODE END 3 */}
And i catch nothing at all, my spi buffer all 16 bytes are 0. I tried SPI_DMA it changed only first byte on 0XFF. What am i doing wrong? Thanks
#stm32f4-spi #receive Note: this post was migrated and contained many threaded conversations, some content may be missing.Solved! Go to Solution.
2018-05-31 5:50 AM
Please zip you code, its very difficult, when you don't have the code and a line number.
2018-05-31 6:06 AM
Hope direct drobox url is ok.
http://dl.dropbox.com/s/gdcq5dpyx31bxwc/SPI%20REGISTERS.zip?dl=0&file_subpath=%2FSPI+REGISTERS
2018-05-31 7:04 AM
we need to see the scope of the whole transaction,
where is the nSS trace ?
EDIT: this is not correct for the SPI slave function:
//////// but you may want to add this line at 114.
/////////// hspi1.Instance->SR = 0; // tx 8 clock cycles to load receiver
/////////// we need to transmit before we can receive.
2018-05-31 7:48 AM
Please check the reference manual page 883, 3.2 Configuring the SPI in slave mode in DocID018909Rev 13
there is a check list,
can you see your incoming data changes as the clock is dropping.
thats either
CPOL = 1 and CPHA = 1;
or
CPOL = 0 and CPHA =0
2018-06-07 2:08 AM
Hello,
I’m going back to begin of this thread to comment your polling example where can see few discrepancies at your code:
Hopefully this would be helpful information for you to continue in the project
Best regards,
Petr
2018-06-08 7:08 AM
Thank you Petr for reply. Actually i solved the problem, but it was test device where speed wasnt too high each clock was around 2us as you can see from the pictures. But real device has 50nanoseconds per clock. And here is a problem, it catches LOW on data and start reading as i wants BUT seems like while MCU procceses the code with HAL_RECEIVE, we are loosing data, seems like HAL really slow, im loosing 2 bytes from the time when i catch zero on data, spi starts reading too late... THis is a code:
while (HAL_GPIO_ReadPin (GPIOA,GPIO_PIN_7) == GPIO_PIN_RESET){} // wait until GPIOC 9 goes high
while (HAL_GPIO_ReadPin (GPIOA,GPIO_PIN_7) == GPIO_PIN_SET){}
//
wait until GPIOC 9 goes low
HAL_SPI_Receive(&hspi1, (uint8_t *)spi_Rxbuffer, 19, 2000);
// read 19 bytes
Actually im not 100% sure that its
HAL_SPI_Receive and not
HAL_GPIO_ReadPin which causes this error. I tried to wait low on data with CMSIS register output which should be much faster, but i struggle with it., im waiting GPIOA.7 -
while((GPIOA->IDR & 0x80) != 0x80) {} - doesnt know does it okay or not. Also i dont know why but after i initialize GPIO pins, IDR register holds 0x00000D40 value, i dont know why. How can i solve it?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.