2013-08-25 5:46 AM
I'm new on STM32F407 and STM32F4xx DSP and Standard Peripherals Library.
And now I've got some question.1) GPIO timing
When I code
GPIOF->BSRRH = 0x0100U;
GPIOF->BSRRL = 0x0100U;
GPIOF->BSRRH = 0x0100U;
GPIOF->BSRRL = 0x0100U;
GPIOF->BSRRH = 0x0100U;
GPIOF->BSRRL = 0x0100U;
I didn't see the desired signal on pin PF8.
When I place some delay between every line it works.
What is the minimum required delay?
Is there another way to force the Output?
2) IS_GPIO_PIN() in stm32f4xx_gpio.h
In stm32f4xx_gpio.h is the macro IS_GPIO_PIN() defined.
#define IS_GPIO_PIN(PIN) ((((PIN) & (uint16_t)0x00) == 0x00) && ((PIN) != (uint16_t)0x00))
But I didn't understand (((PIN) & (uint16_t)0x00) == 0x00).
This is always evaluated to true.
Can somebody explain this condition?
3) assert in GPIO_SetBits(),GPIO_ResetBits()
I use PB0-7 as data bus to an old LCD module.
So I've got the following code
void LcdData(const unsigned char uiData)
{
GPIO_ResetBits(GPIOF, 0x00FFU); //Reset data bus
GPIO_SetBits(GPIOF, uiData); //Set data bus
GPIO_SetBits( GPIOF, 0x0100U); //Set chip select
GPIO_ResetBits(GPIOF, 0x0100U); //Reset chip select
}
When I call LcdData(0x00U) I get an assert().
When I remove this assert it works fine.
Is there a reason that GPIO_SetBits() does not allowed 0x0000U as argument?
4) Not const prove function in Standard Peripherals Library
I try to initialize a port with the following code:
void init(void)
{
static const GPIO_InitTypeDef sInit =
{
GPIO_Pin_0, // uint32_t GPIO_Pin;
GPIO_Mode_OUT, // GPIOMode_TypeDef GPIO_Mode;
GPIO_Speed_2MHz,// GPIOSpeed_TypeDef GPIO_Speed;
GPIO_OType_PP, // GPIOOType_TypeDef GPIO_OType;
GPIO_PuPd_NOPULL// GPIOPuPd_TypeDef GPIO_PuPd;
};
GPIO_Init(GPIOF, &sInit);
}
But the compiler reports an incompatible with parameter
Is there a reason why GPIO_Init() is not declared with const?
void GPIO_Init(GPIO_TypeDef* const GPIOx, GPIO_InitTypeDef* const GPIO_InitStruct);
Many thanks for your answers
Reto Felix
2013-08-25 9:40 AM
1) That's odd, because such code should be able to generate high rate toggling. What compiler are you using, and what code is it generating for this? What bandwidth scope/probes are you using? What speed are the IO ports set too? 100 MHz?
4) Probably because the data structure is frequently not used in the const form, and instead manipulated and changed as part of typical initialization routines.2013-08-25 10:36 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.