2013-08-24 9:41 AM
Hi there,
If I setup both ADC1 and ADC2 in independent mode and set ADC1 to scan channels 1,2,3 using DMA and setup ADC2 for analog watchdog on channel 2 having different sampling times for channel 2 between the two ADCs. Would ADC1 and ADC2 be operating totally independently having absolutely no effect between the two ADCs? ie, if both ADCs happen to want to sample channel 2 at the same time, would one has to wait for the other? or worst corrupt the other's sample, etc...? #adcWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.