STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CS42L52 Codec Configuration on MCBSTM32F400 board

Posted on August 26, 2013 at 15:20 Hi , I am having a little bit of trouble configuring the audio codec (cirrus CS42L52) on the MCBSTM32F400  (stm32f407IG) evaluation board . I am trying to do a reset to the codec via the reset pin , but looking fro...

gdb and external memory

Posted on August 22, 2013 at 16:35Hello Everyone, I am using stm32f407 which is interfaced with 1MB of external RAM. Linker script is a simple one where it puts the data and bss section in external RAM. Regarding code execution I don;t have an issue...

STM32F407 and STM32F4xx DSP and Standard Peripherals Library

Posted on August 25, 2013 at 14:46I'm new on STM32F407 and STM32F4xx DSP and Standard Peripherals Library. And now I've got some question.1) GPIO timingWhen I code            GPIOF->BSRRH = 0x0100U;            GPIOF->BSRRL = 0x0100U;            GPIO...

reto by Associate
  • 1503 Views
  • 2 replies
  • 0 kudos

Are ADC1/2/3 in the F103 totally inedpendent?

Posted on August 24, 2013 at 18:41Hi there,    If I setup both ADC1 and ADC2 in independent mode and set ADC1 to scan channels 1,2,3 using DMA and setup ADC2 for analog watchdog on channel 2 having different sampling times for channel 2 between the ...

bikejog by Associate II
  • 772 Views
  • 0 replies
  • 0 kudos

STM32F2/4 SPI Slave rx DMA and unknown transferlength

Posted on August 23, 2013 at 12:48Hello again, I have connected two STM32F2 via SPI1. The data will be transfered via a variable sized datablock. The first two bytes are a command (5 bit) and a length (11bit) information of the following block. Is i...

mail2 by Associate II
  • 1708 Views
  • 3 replies
  • 0 kudos

ITM_SendChar blocks when no debugger attached?

Posted on August 23, 2013 at 09:39I think ITM_SendChar is freezing my code when I don't have a debugger attachedWhen I do have an debugger attached, it works, and I can see my messagesBut when I don't, then the code doesn't get past the printingBut ...

STM32F10x + EVAL L6470 for stepping motors

Posted on February 07, 2013 at 06:15Hi guys !I'm just about to order but wanted to make sure first. I'm trying to get four stepping motors (bipolar) in daisy chain. I want to use the chain as it is said in AN3991 with the difference that I'll be use...

STM3210E-EVAL + SDIO

Posted on August 23, 2013 at 11:16Good day,Have anybody make it work? I tried the example from:...\STM32F10x_StdPeriph_Lib_V3.5.0\Project\STM32F10x_StdPeriph_Examples\SDIO\uSDCardBut it does not work. I mean reading, writing functions.. I could only...

hitsumen by Associate II
  • 1698 Views
  • 4 replies
  • 0 kudos

Overdriving LSI oscillator by external oscillator

Posted on August 23, 2013 at 15:06Hi everyone,I overdrive the low-speed internal oscillator by external source with a small offset and small swing.Where can I find parameters for external clock(without bypassing LSI osc)?Thanks.Eugene #lsi #oscil...

st2399 by Associate
  • 1382 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.