cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F401 -- SPI Slave Receiving 32bit word

dibs
Associate II
Posted on April 30, 2014 at 23:57

I have a SPI master device that transmits data in 32 bits while NSS is active. Since the STM32F401 SPI can only be configured as a 16bit SPI port, I am wondering if I can still make it work. Will the SPI port continue to receive data in 16 bit increments as long as NSS is held low?

#stm32f4 #spi #32bit
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.