2014-10-30 7:14 AM
Dear Sir/ Madam,
I have just write one program for stm32f401 RE nucleo board in order to read acceleration from KXP84-2050 ( all in rar files). I cannot understand it is alway stuck in send function because i checked with one printf at the end but it not run in Hyperterminal although I followed some codes on the Internet. Therefore, please someone has ever exprience with programming with spi communication for this series is able to help me to fix it.http://www.mediafire.com/download/hc6d6tc8496dini/spi+program.rarWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.