STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F205VB ADC with external reference

Posted on October 30, 2014 at 11:17Hi,I try to use the ADC with ext ref but it doesn't work...I use ADC 1 from PA3.Are there any sample or does have anybody code example? #whiskey-tango-foxtrot

sven by Associate II
  • 1753 Views
  • 4 replies
  • 0 kudos

stm32f10x with AES and CBC

Posted on October 30, 2014 at 16:54Hi Is there an example code or library for the stm32f10x that does AES128 encryption\decryption with CBC cipher mode. thanksLiam

lmullane by Associate II
  • 1020 Views
  • 1 replies
  • 0 kudos

stm32f401 RE connect data with KXP84-2050 through SPI

Posted on October 30, 2014 at 15:14Dear Sir/ Madam,I have just write one program for stm32f401 RE nucleo board in order to read acceleration from KXP84-2050 ( all in rar files). I cannot understand it is alway stuck in send function because i checke...

phivus2 by Associate
  • 532 Views
  • 0 replies
  • 0 kudos

Read stm32f4 device

Posted on October 30, 2014 at 13:31Hi.How can I read device ID with software?Is there any register that stores this value?I would like to detect device on which program is running.Or at least size of flash.I'm using stm32f4 devices.

tm3341 by Associate II
  • 1209 Views
  • 2 replies
  • 0 kudos

Problems with programming LCD (STM32L)

Posted on October 30, 2014 at 10:48I am new to stm32 programming and I am using the STM32L1 Discovery Board (this one http://uk.farnell.com/stmicroelectronics/stm32l152c-disco/stm32l-discovery-eval-board/dp/2317987).I was trying to program the embed...

STM32 UFBGA176+25 Recommended Land Pattern

Posted on October 30, 2014 at 10:45The title says ist all - is there a recommended land pattern for the STM32 UFBGA176+25 package (0.8 pitch)? Can someone share their experience with low-cost prototyping shops like PCB-Pool? #stm32-land-pattern-l...

arne by Associate II
  • 1654 Views
  • 1 replies
  • 0 kudos

Identifying revision of stm32F429

Posted on October 30, 2014 at 12:08Hello, i have bought a stm32f429zit6 and have the suspiction that they delivered me a revision y, but assured me before that they have revision 3 in store. Can you acknowledge that this is revision y? Thanks! Stef...

0690X00000602yhQAA.jpg
sk-st by Associate III
  • 1336 Views
  • 1 replies
  • 0 kudos

XML parser

Posted on October 07, 2013 at 13:12Hello everybody! Is anyone use XML parser at STM32 mikrocontrollers? I search a lot but not found a good for the embedded applications.

totti001 by Associate II
  • 6467 Views
  • 10 replies
  • 0 kudos

EXTI Interrupts with STM32VLDISCOVERY

Posted on January 04, 2014 at 13:40 Hello, I am using STM32VLDISCOVERY and connected 4 tiny push buttons to Pins PB12, PB13, PB14 and PB I am using external pull-up resistors of 100K each (I guess 10K would be much better). Using the...

aa_talaat by Associate II
  • 3915 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.