2013-12-04 1:45 PM
I am attempting to get an STM32F4 to receive data in Master mode. I am getting a problem where the RXNE interrupt is never tripped.
*Should this work, even if you have MISO tied to GND or 3.3V?*Do I need to do anything with the NSS in the peripheral?**Ignore the CS requirements of the slave for now. #stm32f4 #spi2013-12-06 6:41 AM
The rules are:
When TXE set you can write to SPI_DR register (writing the SPI_DR clear TXE bit) When RXNE set you can read from SPI_DR register (reading the SPI_DR clear RXNE bit) You can check the bit status before read to/write from SPI peripheral or you can start an automatic control enabling interrupt/dma ....We’re moving the ST Community to a new platform to give you a better and more reliable community experience.