STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ADC 12bit in STM32f4 discovery

Posted on December 07, 2013 at 17:01Hi. Can you show me ADC register map of  ADC1 and ADC2 12 bit? in example incle lib  ADC3_DR_ADDRESS     0x4001224C. I read manual but can find it. In ADC I see 0x000 - 0x04C ADC1.0x100 - 0x14C ADC2.Thanks

41003160 by Associate II
  • 1725 Views
  • 3 replies
  • 0 kudos

Independent Watchdog Timer

Posted on December 08, 2013 at 14:54hello I want to learn how to use independent watchdog so I wrote this code but it doesnt work .here is my code :#include ''stm32f10x.h''#include ''stm32_eval.h''#include <stdio.h>GPIO_InitTypeDef GPIO_Config_Anaht...

STM32F4-Discovery - problem with debugging in RAM

Posted on December 08, 2013 at 15:56 Hello, I'm using CooCox IDE. I have problem with debugging in RAM and USART communication on STM32F4-Discovery. When I load my program to FLASH all works correctly , data transmit and LEDs on PD12-PD15 switch on ...

st-com by Associate
  • 1287 Views
  • 2 replies
  • 0 kudos

Dynamic Memory Usage

Posted on December 04, 2013 at 12:23Hi guys, I have to do a RAM check routine that performs Class-B controls on pre-assigned (probably all RAM) memory block. The first doubt that rise is : if I allocate the memory statically I can't free it (or rele...

sarraciro by Associate II
  • 5588 Views
  • 9 replies
  • 0 kudos

stlink v2 & ITM trace

Posted on November 07, 2013 at 19:02 Hi, I am currently stuck with stlink v2 and ITM trace on a STM32F103RB. I am using CMSIS debug support by simply calling ITM_SendChar(). This is the only trace specific code than I am using. I...

bernd by Associate II
  • 6252 Views
  • 9 replies
  • 0 kudos

STM32F4 - Master Receive

Posted on December 04, 2013 at 22:45I am attempting to get an STM32F4 to receive data in Master mode. I am getting a problem where the RXNE interrupt is never tripped.*Should this work, even if you have MISO tied to GND or 3.3V?*Do I need to do anyt...

dibs by Associate II
  • 4680 Views
  • 10 replies
  • 0 kudos

WFI returns to unexpected address after DEEPSLEEP

Posted on December 03, 2013 at 23:55Hi, I'm experiencing an odd problem on the STM32F103RF where I get a hard fault UNDEFINSTR on return from WFI in DEEPSLEEP.  Here's a summary of my observations: 1. The hardfault occurs attempting to execute code ...

greg2 by Associate
  • 3681 Views
  • 10 replies
  • 0 kudos

STM32F0-Discovery SPI2 setup and operation.

Posted on December 05, 2013 at 15:02I have an application that requires both of the SPI interfaces running as masters. The code currently has SPI1 up and running. I have then copied the setup function calls and updated them to configure SPI2 (taking...

jason23 by Associate II
  • 2734 Views
  • 4 replies
  • 0 kudos

stm32f429Idiscovery demo touchscreen bug

Posted on December 04, 2013 at 20:29Hello,Today I bought one of  these new stm32f429 discovery boards :http://www.st.com/web/catalog/tools/FM116/SC959/SS1532/PF259090For the moment I only launched the demo software, but it seems that the tuchscreen ...

atsju2 by Associate II
  • 5147 Views
  • 10 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.