2014-01-23 3:49 AM
Hello all,
while implementing two different tasks for DMA2 transfer, which of courseuses different streams and channels I have noticed, that stream initialization sequenceplays some role. For example I am using stream 3 and stream 1 and if I initializefirst stream 3 followed stream 1, then sometimes happens, that data is not transferredin the right way. If start-up sequence initializes first stream 1 followed stream 3 I amnot experiences any troubles. In my case interaction is between DCMI-SDRAM-SDwhich all uses DMA to transfer data.Could someone give me some explanation of this curious case? Since I do not know the reason why is this like explained I am worried, that this is notjust some coincidence and later my fails!Second question is, in what relationship are DMA streams and DMA channels. Like I seenumber of streams are the same as numbers of channels, but in some examples streamnumber does not match channel number! Why this reason? I also tried to change channelnumber and DMA fails. regards2014-01-23 8:08 AM
Without attempting to understand your problem, have you read the Errata, namely item 2.1.10?
JW2014-01-23 1:54 PM
I am not sure to which errata you are referring. My device is STM32F427ZG.
In errata is mentioned SDIO HW flow control, which could bring DCRCFAILwhat I receive, but this flow control is disabled.2014-01-23 7:23 PM
Each stream is a transfer of data between a peripheral and memory. Each DMA can have up to 8 streams active at once. Peripherals are connected to streams via fixed channel assignments. There is a table for each DMA in the F4 reference manual DMA section that identifies these assignments. When you changed channels and the transfer failed, you probably made an incorrect assignment.
Cheers, Hal2014-01-23 11:34 PM
> I am not sure to which errata you are referring. My device is STM32F427ZG.
Ah. I was referring to errata to the 40x/40x sub-group - it appears to have a bug specific to DMA2 serving peripherlas with built-in FIFO (DCMI, CRYPTO, and HASH). There is no such bug mentioned in the '427 errata. JW2014-02-18 8:16 AM
Hello all,
Have you seen the new application note AN4031 describing how to use DMA with STM32F2 & STM32F4 products? You can find it on this link:http://www.st.com/web/en/resource/technical/document/application_note/DM00046011.pdf
. Hope it will be helpful in this case. Don't hesitate to let us know your feedbacks. -Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.