2014-02-18 2:59 AM
I'm working with the STM32F051
I have this code which works for usart1 but not for usart2.appreciate any help-Gilad#include ''stm32f0xx.h''#define UART2#ifdef UART1 #define USARTx USART1 #define DATA 0x31#else #define USARTx USART2 #define DATA 0x32#endifvoid main(void){ GPIO_InitTypeDef GPIO_InitStructure; USART_InitTypeDef USART_InitStructure; /* Enable GPIO A clock */ RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);#ifdef UART2 /* Enable USART2 clock */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE);#else /* Enable USART clock */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE); /* Configure the HSI as USART clock */ RCC_USARTCLKConfig(RCC_USART1CLK_HSI);#endif /* Configure USART Rx & Tx as alternate function */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9 | GPIO_Pin_10; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_Level_3;//GPIO_Speed_40MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init(GPIOA, &GPIO_InitStructure); /* Mux out USART2 Rx & Tx */ GPIO_PinAFConfig(GPIOA, GPIO_PinSource9, GPIO_AF_1/*GPIO_AF_USART2*/); // PA2 USART2_TX GPIO_PinAFConfig(GPIOA, GPIO_PinSource10, GPIO_AF_1/*GPIO_AF_USART2*/); // PA3 USART2_RX USART_InitStructure.USART_BaudRate = 115200; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No;//USART_Parity_None; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; /* USART configuration */ USART_Init(USARTx, &USART_InitStructure); /* Enable USART */ USART_Cmd(USARTx, ENABLE); while(1) { while(USART_GetFlagStatus(USARTx, USART_FLAG_TXE) == RESET); /* Waitwhile TX full */ USART_SendData(USARTx, DATA); }}2014-02-18 3:53 AM
Hi
''#ifdef UART2 /* Enable USART2 clock */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE); #else /* Enable USART clock */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE); /* Configure the HSI as USART clock */ RCC_USARTCLKConfig(RCC_USART1CLK_HSI); #endif'' Why are you not setting the USART clock for USART2?2014-02-18 5:31 AM
/* Enable USART2 clock */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE);
2014-02-18 6:26 AM
Hi
'' /* Configure USART Rx & Tx as alternate function */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9 | GPIO_Pin_10; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_Level_3;//GPIO_Speed_40MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init(GPIOA, &GPIO_InitStructure);'' One problem is that USART2 does not come out on the same pins as USART1 USART 2 comes out on PA2 and PA3 or PA14 and PA15We’re moving the ST Community to a new platform to give you a better and more reliable community experience.