STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32429I-EVAL Drivers & Example software?

Posted on February 06, 2014 at 16:29Hi,I've recently started developing on the STM32429I-EVAL board. The user manual mentions 'demonstration software', but I'm unable to find the source online. I'm fairly new to developing for ST boards, am I right ...

thomas2 by Associate II
  • 2961 Views
  • 6 replies
  • 0 kudos

STM32F4 DMA streams init sequence

Posted on January 23, 2014 at 12:49Hello all,while implementing two different tasks for DMA2 transfer, which of courseuses different streams and channels I have noticed, that stream initialization sequenceplays some role. For example I am using stre...

usart2 problem

Posted on February 18, 2014 at 11:59I'm working with the STM32F051 I have this code which works for usart1 but not for usart2.appreciate any help-Gilad#include ''stm32f0xx.h''#define UART2#ifdef UART1  #define USARTx USART1    #define DATA 0x31#else...

gilad by Associate
  • 1679 Views
  • 3 replies
  • 0 kudos

STM32F429 SPI4 via DMA

Posted on February 06, 2014 at 11:50Hello everyone,I'm using the SPI4 to read out data from an SD-card, witch is working. Now I want to let the DMA controller do the work at least I want him to do it... I pretty much used the code of the F4 discover...

p23 by Associate II
  • 2023 Views
  • 4 replies
  • 0 kudos

USB interface association descriptor

Posted on February 18, 2014 at 09:39Hello, I have made a 'two-in-one' device using an USB interface association descriptor: a generic HID, and a streaming audio device. Everything is working as expected, but the device is unstable. When fetching dat...

STM32L15x TIM5 Internal Trigger (ITR)

Posted on February 18, 2014 at 03:18In RM0038 Table 66 (page 379) the Internal trigger connections (ITR) has no entry for TIM5. There's no text describing any functional differences for TIM5 over TIM[234] with respect to these ITR connections, nor d...

greg2 by Associate
  • 1370 Views
  • 2 replies
  • 0 kudos

Samsung 128Mbytes NAND flash ?

Posted on February 14, 2014 at 13:17Guys    Does anyone know where I can find a library for 128Mbytes NAND flash from Samsung ?  thanks for the info

Dead time generation STM32F030K6

Posted on February 15, 2014 at 21:53This software is not working with STM32F030K6 , but this sofware works with STM32F030R8. Prototype 1 used the discovery board. No we made a PCB with STM32F030K6. And the code is not working anymore. Makes reset. ...

franz2 by Associate III
  • 1206 Views
  • 2 replies
  • 0 kudos

Cannot install STM32W Composite Device

Posted on January 23, 2013 at 07:03Hi, Yesterday i have taken a STM32W RFC kit, in the user manual of RFC kit in section 1.8.2 it is given that ''To use the serial communication channel on the kit application boards, a Virtual COM port driver for S...

gopallal by Associate
  • 3371 Views
  • 8 replies
  • 0 kudos

SM32F407 Discovery + HID + COOS

Posted on February 16, 2014 at 23:00I'm planning a prototype using HID and coOS, using coIDE, and would like to know if somebody tried before those products together.Thanks in advance. Best regards. #go-to-the-horse's-mouth

carlos2 by Associate
  • 1059 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.