2014-01-15 1:19 AM
Hi,
I'm trying to communicate between the
http://www.ti.com/product/ADS7870
and the ST microcontroller STM32F4 Discovery evaluation board. I'm using IAR and at the moment I'm just trying to read register 31 from the ADC (which should return a 1) but with no luck.I'm setting the SPI on the microcontrontroller as follows: data transmitted as MSB first, clock low in idle state, data is captured on rising edge, data size is 8 bits, and full duplex transmission.
In main.c I do:
http://e2e.ti.com/support/data_converters/precision_data_converters/f/73/t/3147aspx#
1
2
3
4
5
6
debug = ads7870Init();
if
(debug==1)printf
( ''adc is alive \n'' );else
printf
( ''adc is DEAD \n'' );And in
http://www.ti.com/product/ads7870
_driver.c I have:http://e2e.ti.com/support/data_converters/precision_data_converters/f/73/t/3147aspx#
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
//initialize ADC
uint8_t ads7870Init( void ) {//// check ID register
if
(ads7870ReadReg(ADS7870_ID) != ADS7870_ID_VALUE)return
0;else
{
//// setup reference and buffer
ads7870WriteReg(ADS7870_REFOSC, ADS7870_REFOSC_OSCE | ADS7870_REFOSC_REFE | ADS7870_REFOSC_BUFE);
//// return success
return
1;}
}
I'm attaching a screenshot of what I see on the scope. (yellow: sclk, blue: read command register 31, purple: output from ADC).
MOSI transmits properly to the
http://www.ti.com/product/ADS7870
(the din pin receives read command), but there is no response coming from the ADC dout pin.I would really appreciate any help on this.
Thank you.
2014-01-17 2:47 AM
No, I will try that on Monday when I'm with the device. Thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.