2015-01-22 4:27 PM
An application which includes DMA over SPI communication protocol is running nicely once STM32F405 is powered up. However, once running the same code from debugger - it does NOT behave properly.
What might be the cause(s) for the difference?Some more info: The debugger is an IAR I-jet and the development tool is Workbench IDE 7.30. CPU system clock is 36MHz from the HSI. #stm32f4-debugger-initializationWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.