STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32f4-discovery with STM32CubeMX

Posted on January 15, 2015 at 14:34Hello, I am using an stm32f4-discovery board with MCU stm32F407. My intention is create a project using the STM32CubeMX c generator using both RTOS and USB Middlewares. I want to be able to see in my Device Manager...

ilias by Associate II
  • 1752 Views
  • 3 replies
  • 0 kudos

User error: Reset failed - Target held in reset state

Posted on January 21, 2015 at 07:04Hi All,         I am trying to program STM32F105RCT7 using IAR, while I do program I am facing an error as belowUser error: Reset failed - Target held in reset state.      I have check voltages at pin no. 1, 13, 19...

maulin by Associate II
  • 4414 Views
  • 8 replies
  • 0 kudos

STM32F4 DISCOVERY CAN bus controller problem

Posted on July 13, 2012 at 15:57Hi all,I am trying to get the CAN interface working on the STM32F4DISCOVERY board.After calling the configuration functions from the peripheral library, when I tried to transmit message with just a oscilloscope connec...

USART In Synchronous Mode: SOME Data Incorrect

Posted on January 22, 2015 at 19:46Now that I've got my USART working with my DMA to do two 8-bit transfers per 16-bit word, I have encountered another problem: incorrect data. I know the mantra for serial comms when data is wrong is baud rate, baud...

jvavra by Associate III
  • 865 Views
  • 1 replies
  • 0 kudos

STM32F4 UART IRQ issue

Posted on January 22, 2015 at 10:07 Hi, I am trying to receive RF packet using USART1 IRQ, using below code. But packets are missing in the receive end. My point here is sometimes i will receive packets and the received packet is completely...

vivek23 by Associate II
  • 1931 Views
  • 4 replies
  • 0 kudos

STM32F4 different run from chip vs Debugger

Posted on January 23, 2015 at 01:27An application which includes DMA over SPI communication protocol is running nicely once STM32F405 is powered up. However, once running the same code from debugger - it does NOT behave properly. What might be the c...

isaac by Associate II
  • 748 Views
  • 0 replies
  • 0 kudos

ST32F4xx custom bootloader in top sector of flash

Posted on January 22, 2015 at 06:55ST32F415 to be exact. Boot ROM disabled by BOOT0 jumper. I saw a product where a custom bootloader was flashed into sector 11 (highest in that chip). And a reset vectors to that bootloader. User code goes in sector...

USB on stm32f103

Posted on January 20, 2015 at 00:39 Hi, I'm trying to use a mass storage example taken from here http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1743/LN1734/PF258157. When I'm executing, at startup the driver gets a S...

geoffrey by Associate II
  • 1988 Views
  • 4 replies
  • 0 kudos

stm32f4 discovery timer 1 frequency issue

Posted on January 18, 2015 at 20:43 Hi, I am using stm32f4 's timer 1 in pwm mode.I configured the board frequency using the excell clock configuration tool. I managed to provide TIM1 a clock source of 8 MHZ. Then i put 20 in timer 1 's pr...

d4ng3r09 by Associate II
  • 1891 Views
  • 4 replies
  • 0 kudos

''Simulate'' 16-bit SPI Transfer w/ USART in Synchronous?

Posted on January 06, 2015 at 20:19I've got a project with three ASICs that expect 16-bit words to be received via SPI, transferred via DMA . Unfortunately, due to a pin conflict, I only have SPIs 1 and 3 available. So. I was thinking about trying t...

jvavra by Associate III
  • 1436 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.