2015-10-15 9:54 AM
2015-10-15 10:45 AM
So is this an Arduino question, or an STM32 one?
From the STM32 you might want to double check the frequency the part is running at, and the frequencies of the APB. Output the clock via MCO (PA8) and confirm. Check also with RCC_GetClocksFreq()2015-10-15 12:47 PM
First, thank you clive1. I want the send data from arduino to Stm32f4 with Can-Bus.
My application APB Clock=42 Mhz , PLL_M=8 Mhz and PLL_N=336 Mhz. So, HSE_VALUE=8 Mhz. I want to send data from STM32F4 to Arduino Uno. Its work Master and Slave. (STM32F4 as Master and Arduino as Slave)Could it be different time quanta value for Arduino and STM32F4? STM32F4 is working 125 KBPS. I check with Logic Analyzer. There is no problem. But, the sent data from Arduino, STM32F4 does not any detect .We’re moving the ST Community to a new platform to give you a better and more reliable community experience.