STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32f4 discovery SDIO write block got cry failed

Posted on October 15, 2015 at 16:34I'm porting SDcard code from FatFS_uSD_FreeRTOS for stm32446_eval in STM32Cube to stm32f4-discovery.Reading blocks seems fine, but writing blocks failed.I debugged with GDB. when write it returned crc failed.here i...

sprhawk by Associate II
  • 985 Views
  • 1 replies
  • 0 kudos

How to use the Virtual Com via ST-Link

Posted on October 12, 2015 at 23:51I have an Discovery board. It has the provision to pass the UART of the target through the on-board ST-Link. I have searched the literature on the board and the manuals. I havent been able to find how this works. I...

rbenesh by Associate II
  • 2300 Views
  • 4 replies
  • 0 kudos

Timer to measure PWM signal and redirect to another GPIO

Posted on October 08, 2015 at 21:45I want to create a PWM pass-through program that will read a PWM duty cycle from an RC receiver on a pin (Pulse-width: 1ms-2ms @ 50Hz) and then output that duty cycle on another GPIO Pin at 50Hz. (eventually, the p...

scook116 by Associate II
  • 1226 Views
  • 2 replies
  • 0 kudos

calcul frequency of PWM signal

Posted on October 15, 2015 at 17:56 hi all membres i try to do a code which calculate the frequency of PWM signal i try with this code but i cant get the right frequency note : i use stm32f429ZIT dicovery /* stm32f429ZIT discovery */ ...

Global/local interrupts in CubeMX?

Posted on September 01, 2015 at 00:51There is a checkbox named USART1 global inrterrupt in Cube NVIC settings. Are there any local interrupts? I used settings for F100 cpu.

LMI2 by Lead
  • 2457 Views
  • 5 replies
  • 0 kudos

STM32CubeMX HAL_I2C_MODULE_ENABLED

Posted on October 06, 2015 at 17:44If I build a Cube config using the stm32f303vctx processor and enable an I2C port, I get HAL_I2C_MODULE_ENABLED in the sources and a hal_i2c include file included. However, if I use the 'stm32f3discovery' board pro...

artgodwin by Associate II
  • 2063 Views
  • 3 replies
  • 0 kudos

stm32f2 SD card corruption

Posted on October 12, 2015 at 17:02Hi to all, Did anybody experience random corruption of bits (not byte) on a SDcard..?We are using an stm32f217 with RTX, FlashFS and tcp from Keil, v4.70. uSD card is connected through SDIO port.We are using 2Gb uS...

STM32F3 Discovery - ADC Calibration Error

Posted on June 19, 2013 at 22:17I'm trying to run the ADC Example code that came along with this board, but I keep getting stuck in a loop where the calibration bit (ADC1.CR - bit 31 of the control register) isn't getting set back to zero, and I'm g...

mattfox by Associate II
  • 5768 Views
  • 15 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.