2015-04-01 2:51 AM
Hello,
I'm stucked and want to ask for some clues.I'm building an 4-phase interleaved boost converter and I need to run a 4-channel PWM with phase shift (90 degree on each channel) and variable duty cycle (same for all channels).I tried to use OC Toggle Mode, but I was unable to change duty cycle.In PWM1 I was unable to phase shift.I tried to use one timer at 4xfreq and then in interrupts fire 4 separate timer, but it wasn't accurate.Will appreciate for any hints, becouse I'm trying to manage it for a week. #phase-shift #pwm #stm322015-04-01 4:36 AM
TIM+DMA pattern buffer into GPIOx->BSRR
2015-04-07 2:13 AM
Clive1 sir,
Could you tell sth more about your proposition or maybe provide any code example?2015-04-07 9:16 AM
I believe I've posted several DMA to/from GPIO pin examples using either internal or external clock sources. The BSRR would allow you to set and clear specific pins within a GPIO bank, from a table, in a timed and sequenced fashion. The periodicity of the timer could be pulled in/out to change frequency, and the pattern/table adjusted to support different duty and phase relationships.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.