2026-02-22 9:19 PM
I’m currently working with an STM32F4 series MCU and using UART with DMA for receiving data from an external module.
The incoming data packets are variable length and don’t always end with a fixed delimiter. Right now I’m using:
HAL_UART_Receive_DMA()
Circular DMA mode
IDLE line interrupt to detect end of frame
However, I’m noticing occasional frame misalignment when packets arrive back-to-back with minimal delay.
A few questions:
Is using the UART IDLE interrupt still considered the most reliable method for variable-length packet detection?
Would switching to LL drivers improve timing control significantly in high-throughput scenarios?
Are there recommended buffering strategies to avoid data corruption when processing data inside the IRQ context?
System details:
MCU: STM32F4
Baud rate: 115200
No RTOS currently
Processing happens in main loop
Any advice or production-proven approaches would be appreciated.
Thanks!
2026-02-23 12:05 AM
Hello there,
The F4's IDLE interrupt missing back-to-back packets is a known hardware limitation as my knowladge, as it requires at least one full frame of silence to trigger. To make your system solve this problem, you shouldn't rely on the IDLE interrupt to perfectly frame your packets.
Instead, set up a large DMA circular buffer (which I belive you have it). Use the IDLE, Half-Transfer (HT), and Transfer Complete (TC) interrupts only to update a software 'write pointer' (reading the DMA NDTR register directly via LL macros is much faster here than HAL as you asked). Then, in your main while loop, treat that circular buffer as a continuous raw byte stream. Feed those bytes into a software State Machine that actively looks for your packet headers, length bytes, and CRCs. This way, even if packets get glued together by the DMA, your parser will slice them apart accurately.
Note: I work F7 and H7 and they have receiver timeout proporties and it helps to provide this problem.
2026-02-23 5:58 AM - edited 2026-02-23 5:59 AM
Use HAL_UARTEx_ReceiveToIdle_DMA which will call the HAL_UARTEx_RxEventCallback callback on the HT, TC and IDLE flags. This is the most reliable way.
Here is an example to go from:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.