2016-11-04 4:42 AM
I've compiled and linked the original sources without modifications of the board. After upload and starting the demo with the debugger the initialisation should start with LED3.
here the code snipped:/* Initialize LEDs and User Button available on STM32F3-Discovery board */
STM_EVAL_LEDInit(LED3); STM_EVAL_LEDInit(LED4); STM_EVAL_LEDInit(LED5); STM_EVAL_LEDInit(LED6); STM_EVAL_LEDInit(LED7); STM_EVAL_LEDInit(LED8); STM_EVAL_LEDInit(LED9); STM_EVAL_LEDInit(LED10); STM_EVAL_PBInit(BUTTON_USER, BUTTON_MODE_EXTI); /* Configure the USB */ Demo_USB(); /* Reset UserButton_Pressed variable */ UserButtonPressed = 0x00; Stepping through the code until LED10 all led's should be light on in the order where they are initialised. But this doesn't happen. The order where the led's begin to go on is: LED4 -> LED3 -> LED5 -> LED7 all other LEDs remain off. Stepping unit the call Demo_USB() the function dos not return the while-statement: while ((bDeviceState != CONFIGURED)&&(USBConnectTimeOut != 0)) {} Don't know why this happen, any hint ? Thanks for help.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.