cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G0B1CBT3N vs STM32G0B1CBT6N

Tintin33
Associate

Hello Peter , 

Need your expert reply 

As we see , the confusion on N AND no N HAS MADE many of us wonder , if these can be used as  interchangeable parts . Since Data Sheet does not explain , much on them ,But a search explains a compact Solution in Io's for a design flexibility . 

As both have same Packages and Pin  Count . 

We are in need for DESIGN - STM32G0B1CBT3N , but seems to be difficult  to procure  . Is this Manufactured or is it rare . We only See STM32G0B1CBT6N 

 

Regards

Nitin

1 REPLY 1
Peter BENSCH
ST Employee

Welcome @Tintin33, to the community!

By looking at the product website for the STM32G0B1CB, it can be seen that there is currently no STM32G0B1CBT3N (-40...+125°C). At present, therefore, you only have the option of using the STM32G0B1CBT6N (-40...+85°C).

If you absolutely need the wider temperature range, you will need to clarify availability with your local distributor, which will in any case require a minimum order quantity to release this variant - assuming that this is even possible at high temperatures because of the added functionality (VDDIO2 and UCPD).

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.