2015-03-15 7:22 AM
Hi guys,
Sorry to trouble you frequently. Can't help!! I have an STM32F105VC (100 pin device). Trying to use I2C bus on pins 95, 96. This is I2C1 (PB8, PB9) and requires remap (as per documentation). Did the following init. Not able to read or write. Here is the init code. Same code without remap but on I2C2 worked on a 64 pin device (STM32F103RC). void I2C1_Configure (void) { // First remap pins. GPIO_PinRemapConfig(GPIO_Remap_I2C1,ENABLE); GPIO_InitStructure.GPIO_Pin = I2C_EE_SCL | I2C_EE_SDA; // GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8 | GPIO_Pin_9; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_OD; GPIO_Init(GPIOB, &GPIO_InitStructure); /* I2C configuration */ I2C_InitStructure.I2C_Mode = I2C_Mode_I2C; I2C_InitStructure.I2C_DutyCycle = I2C_DutyCycle_2; I2C_InitStructure.I2C_OwnAddress1 = 0xF0; I2C_InitStructure.I2C_Ack = I2C_Ack_Enable; I2C_InitStructure.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit; I2C_InitStructure.I2C_ClockSpeed = 80000; I2C_Init(I2C1, &I2C_InitStructure); /* I2C Peripheral Enable */ I2C_Cmd(I2C1, ENABLE); }2015-03-16 6:26 PM
Well after some searching I found that there is a bug in the device (105) itself. Any one facing similar problem, please go through errata of the particular device (or is it better/safer to go through the errata before choosing a device). I have implemented the workaround suggested in the errata and it started working but not without a problem. Thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.