2015-01-02 6:56 AM
I'd like to present real-time kernel:
https://bitbucket.org/dfrank/tneokernel
. TNeo was born as a thorough review and re-implementation of . The new kernel has well-formed code, inherited bugs are fixed as well as new features being added, it is well documented and tested carefully with unit-tests. Currently it is available for the following architectures:Comprehensive documentation is available in two forms:
Short list of features can be found
. #kernel2015-03-16 4:34 PM
TNeo v1.07 is released, this is a minor release with a few bugfixes and some new features.
Changelog is available here:http://dfrank.bitbucket.org/tneokernel_api/dev/html/changelog.html
Downloads here:We’re moving the ST Community to a new platform to give you a better and more reliable community experience.