2012-05-06 8:18 AM
Hi i stay try to send a character from Hyperterminal on the usart without any control on flow of usart(HW control or Xon/Xoff control)
this is my code#define RCC_APB2ENR *(long*) 0x40021018#define GPIOA_ODR *(long*) 0x4001080C#define GPIOB_ODR *(long*) 0x40010C0C#define GPIOA_CRH *(long*) 0x40010804#define GPIOB_CRH *(long*) 0x40010C04// Define for USART_RS232#define USART1_SR *(long*) 0x40013800#define USART1_BRR *(long*) 0x40013808#define USART1_DR *(long*) 0x40013804#define USART1_CR1 *(long*) 0x4001380C#define USART1_CR2 *(long*) 0x40013810#define USART1_CR3 *(long*) 0x40013814#define USART1_GTPR *(long*) 0x40013818int main (void){ RCC_APB2ENR=0x400C; //Set USART1 GPIOB GPIOA GPIOA_CRH=0x4B0; //PA9 Altenate OUTPUT PA10 Floating INPUT GPIOB_CRH=0x22222222; //Out led at 2 MHz USART1_SR=0x00000000; USART1_BRR=0x0340; //Baud Rate a 9600 USART1_CR1=0x0000200C; // UE, TE, RE USART1_CR2=0x00000801; // Clock Enabled e indirizzo 0001 USART1_CR3=0x00; USART1_GTPR=0x00; while(1) { while((USART1_SR&&0x00000020)==0x00000020) //Control RNXE flag {USART1_DR=0x43; //character control if(USART1_DR==0x41) {GPIOB_ODR=0x005500; //If receive A ODR on portB is 5500 } if(USART1_DR==0x42) //If receive B ODR on portB is AA00 {GPIOB_ODR=0x00AA00; } } }}...i not Know how read correctly from USART_DR or i not set properly for take data from the shift register2012-05-06 9:33 AM
while((USART1_SR&&0x00000020)==0x00000020) //Control RNXE flag
Too many '&' there for a bitwise AND. while((USART1_SR & 0x20)==0x20) //Control RXNE flag The DR is 16-bit wide, you should load it into a variable and then compare the variable. i = USART1_DR & 0xFF; if ((i == 'X') || (x == 'x')) puts(''Pressed X'') else if ((i == 'Y') || (i == 'y')) puts(''Pressed Y''); else if ((i == 'Z') || (i == 'z')) puts(''Pressed Z''); Bit of advice, use the library it'll save a lot of wasted dev/debug time. Mask new data on to peripheral registers, don't blind write over previous configurations.
2012-05-06 1:07 PM
Hi clive1!
Thank you for your help!I've change the while and write only one '&', set i=USART1_DR&0xFF and the if, and not work :-(.I've try also to give in output on Usart the C character and i receive in loop the C, also if i keep pressing for some time the character A or B the status of led change ( I suppose that saturated the shift register).I can't use the library because the prof have tell us to not use them.Thanks for your help!2012-05-06 8:04 PM
Well your teacher seems stuck in 1980, I apologize.
Try this to output a stream of 'C's, I didn't check the addresses, but you do want them to be volatile.#define RCC_APB2ENR *((volatile long*) 0x40021018)
#define GPIOA_ODR *((volatile short*) 0x4001080C)
#define GPIOB_ODR *((volatile short*) 0x40010C0C)
#define GPIOA_CRH *((volatile long*) 0x40010804)
#define GPIOB_CRH *((volatile long*) 0x40010C04)
// Define for USART_RS232
#define USART1_SR *((volatile long*) 0x40013800)
#define USART1_BRR *((volatile long*) 0x40013808)
#define USART1_DR *((volatile long*) 0x40013804)
#define USART1_CR1 *((volatile long*) 0x4001380C)
#define USART1_CR2 *((volatile long*) 0x40013810)
#define USART1_CR3 *((volatile long*) 0x40013814)
#define USART1_GTPR *((volatile long*) 0x40013818)
main()
{
RCC_APB2ENR |= 0x400C; // Clock Enable USART1 GPIOB GPIOA
GPIOA_CRH |= (GPIOA_CRH & 0xFFFFF00F)|0x4B0; //PA9 Alternate OUTPUT PA10 Floating INPUT
GPIOB_CRH = 0x22222222; //Out led at 2 MHz
USART1_BRR =0x0341; //Baud Rate a 9600 @ 8 MHz
USART1_CR1 =0x0000000C; // TE, RE
USART1_CR2 =0x00000000;
USART1_CR1|=0x00002000; //USART ENABLE
while(1)
{
while((USART1_SR & 0x40)==0);
USART1_DR='C';
}
}
2012-05-07 7:25 AM
''I can't use the library because the prof have tell us to not use them.''
I trust that's just because he wants you to understand what it's like to work at the register level? As general advice, as clive1 says, it is rather poor and outdated. Anyhow, the source code of the library is provided - so you can look at the library examples, and see how they do it...2012-05-08 6:43 AM
Hii neil.andrew and clive1,
Thanks for your helps!!!yesteday i'm goed to university and the prof have correct me. I've not impremented well the RS232 protocoll and now work!
#define RCC_APB2ENR *(long*) 0x40021018
#define GPIOA_ODR *(long*) 0x4001080C #define GPIOB_ODR *(long*) 0x40010C0C #define GPIOA_CRH *(long*) 0x40010804 #define GPIOB_CRH *(long*) 0x40010C04 // Define per USART_RS232 #define USART1_SR *(long*) 0x40013800 #define USART1_BRR *(long*) 0x40013808 #define USART1_DR *(long*) 0x40013804 #define USART1_CR1 *(long*) 0x4001380C #define USART1_CR2 *(long*) 0x40013810 #define USART1_CR3 *(long*) 0x40013814 #define USART1_GTPR *(long*) 0x40013818 int main (void) { int IN=0; RCC_APB2ENR=0x400C; //Enable USART1 GPIOB GPIOA GPIOA_CRH=0x8B0; //PA9 Altenate OUTPUT PA10 Floating INPUT GPIOB_CRH=0x22222222; //Out led at 2 MHz USART1_SR=0x00000000; USART1_BRR=0x0340; //Baud Rate 9600 @8Mhz USART1_CR1=0x0000200C; // Enable UE, TE, RE while(1) { while(!(USART1_SR & 0x00000020)); IN=USART1_DR; if(IN==0x41) GPIOB_ODR=0x005500; if(IN==0x42) GPIOB_ODR=0x00AA00; USART1_DR=USART1_DR+2; //Give in Output Rx+2 } }2012-05-08 7:26 AM
I would generally avoid reading the DR multiple time, as it has side effects.
USART1_DR=IN+2; //Give in Output Rx+22012-05-08 7:44 AM
Ok Clive1. I change the code and read the value from IN variable :)
Thank you very much for your help.My next step is the adc1 setting and reading!i'm happy to know that there are people as you on the ST communities.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.