2012-05-08 9:13 AM
Hello,
I've used the code from the example VBAT_Mesurement to test the ADC. Instead of connecting a battery on pin VBAT I've connected VDD 3.3V. The program requests cyclic the converted value. .... VBATVoltage = (ADCConvertedValue*2)*3300/0xFFF; ... VBATVoltage varies from 3287 to 2992. this is a difference about 8 percent. I've checked the power VDD with an oscilloscope , which is quit clean. There are no peaks visible. Does anybody know the reason for this ? Regards, Harald2012-05-08 12:44 PM
Does anybody know the reason for this ?
Using 15 cycle mode I'm seeing +/- 20%, this drops below +/- 1% in 480 cycle mode. ADC_SampleTime_480Cycles2012-05-08 10:36 PM
Thanks,
it works HaraldWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.