2012-06-14 6:55 AM
On the STM32F103C8 chip I can use the PA9 default alternate function to use either USART1_TX or TIM1_CH2 on that pin depending upon which peripheral is enabled.
If both peripherals are enabled and I am using PA9 as USART1_TX, does this preclude me from using TIM_CH1, TIM_CH3, or TIM_CH4?
This assumes that TIM_CH2 is disabled: TIM1 MOE =1 OSSR = x CC2E = 0 CC2NE = 0 I pretty sure the answer is ''Yes'', but would like confirmation. Thank you. #stm32
2012-06-14 7:34 AM
Each pin is independent as to alternate function, so the other timer channels are available.
Cheers, Hal2012-06-14 10:43 AM
Many Alternate Functions can be ''re-mapped'' onto different pins...
2012-06-14 11:04 AM
Many Alternate Functions can be ''re-mapped'' onto different pins...
And sometimes must be otherwise pins clash. This is the case for one of the CAN outputs and a USART CTS or RTS pin. It's in the errata now, but banged my head on it with a 103 design. You need to remap the CAN off in the weeds. PA11 or PA12 as I recall. Definitely review the errata as you floor plan the pin escape of your design.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.