STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Test if running STM32 under debugger.

Posted on June 11, 2012 at 13:10STM32F103RE I'm using the 2 wire serial debug pins as GPIO under normal operating conditions, the JTAG/SW functionality gets disabled early in the main function.  Obviously this would prevent debugging as the debugger...

STM32F103T8 usart2 corrupted data

Posted on September 28, 2011 at 08:12Hi,Im trying to get the usart2 working but for some reason I get random corrupted data when I send message to the STM32F103T8. I can send messages from the STM32 to the computer without any corrupted bytes but no...

mikaeleg by Associate II
  • 5007 Views
  • 11 replies
  • 0 kudos

stm32l152V8t6 pb4-lcdseg8

Posted on May 24, 2012 at 10:56Hi, I'm using the emdedded stm32l lcd driver on the stm32L152V8t6 (lqfp 100pin)   all segments work well,but on the pb4-lcdseg8 I see a fixed voltage level(about 2.9V) very near to the vdd voltage. the lcd glass is ok....

Best ADC conversion method and clamping?

Posted on June 14, 2012 at 03:33Hi Guys, I'm designing a 3-phase DTC induction motor control which needs the 3-phase voltages and 2 of the currents. I am using the STM32F4 Discovery board. The control will have a small sample time (5uS). The control...

0690X00000602l8QAA.jpg

STM32F103C8 Peripheral Alternate Function

Posted on June 14, 2012 at 15:55On the STM32F103C8 chip I can use the PA9 default alternate function to use either USART1_TX or TIM1_CH2 on that pin depending upon which peripheral is enabled.If both peripherals are enabled and I am using PA9 as USA...

markbell9 by Associate II
  • 1723 Views
  • 3 replies
  • 0 kudos

FSMC failure

Posted on June 13, 2012 at 09:35Hi, i am newby with arm cortex m3. I am working on STM32F101xC and i have this problem: driving a lcd with 8080 interface with FSMC i have no problem with st-link debugging and after a ''reset pin'' reset. After power...

Slider used as 4 buttons on STM32L-Discovery

Posted on May 25, 2012 at 15:58Hi,I am new to this forum and I am programming the STM32L-Discovery using Crossworks.I am currently trying to do something which I believe should be relatively simple. e.g when I touch the 1st quarter of the slider - d...

gavin2 by Associate II
  • 1481 Views
  • 4 replies
  • 0 kudos

DAC and ADC issue

Posted on January 27, 2012 at 09:48Update:Ok quick update I have now edited my code to only use DMA with the ADC and software trigger (DAC_SoftwareTriggerCmd) the DAC and it works fine. Therefore it seems to be a DMA issue. The new implementation I ...

eamonn by Associate II
  • 1590 Views
  • 2 replies
  • 0 kudos

Binary Image protection

Posted on June 10, 2012 at 19:07Hi there, I would like to know if there is a way to protect your binary image in a stm32f device (with mpu). With protection i mean that i would like to secure the binary image that runs on the device from been stolen...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.