2026-01-20 8:12 PM
Hello Sir,
I would like to request your guidance regarding the use of an STM32F103 microcontroller as an ST-LINK programmer. I have already flashed a bootloader HEX file intended for ST-LINK functionality into the STM32F103 device. However, I would like to confirm the following points: Is any additional driver, firmware, or configuration file required on the PC side or MCU side to make the STM32F103 work properly as an ST-LINK programmer? Is the flashed bootloader alone sufficient, or are there any specific steps or tools recommended by ST to complete the setup? Could you please provide or point me to the official/original ST-LINK bootloader or firmware source for STM32F103, if available? Are there any reference documents or application notes that explain this implementation in detail? Your support and clarification on this matter would be highly appreciated. Thank you for your time and assistance.
2026-01-20 8:26 PM
The official ST-Link firmware and source code are not distributed.
For official ST-Link programmers, you will also need drivers on the PC as well as a suitable program such as STM32CubeProgrammer for them to work.
STSW-LINK009 | Software - STMicroelectronics
2026-01-21 1:52 AM - edited 2026-01-21 1:53 AM
As @TDK said, ST do not release the ST-Link firmware - see:
So anything you do have is not legitimate.
Therefore there is no support for creating your own "clone" ST-Link.
Note also that ST tools may detect unofficial/unauthorised ST-links, and may not work properly/fully with them.
If you really must make a DIY debug probe, there are open-source projects available; see:
2026-01-22 8:33 PM
WE JUST KNOW ABOUT HOW CAN WE USE A FRESH MCU STM32F103 AS A ST LINK PROGRAMMER JUST LIKE A NUCLEO BOARD PROGRAMMER .
2026-01-22 9:03 PM
You can't.
2026-01-23 1:47 AM
PLEASE DON'T SHOUT!
@vd3 wrote:WE JUST KNOW ABOUT HOW CAN WE USE A FRESH MCU STM32F103 AS A ST LINK PROGRAMMER
And that has been explained to you by both @TDK and me.
Which part is unclear?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.