2018-02-21 4:01 AM
Hi;
I have a problem.
I want to be output pins PC14 and PC 15, so make the registers PWR -> CR = 0x00000100, RCC-> BDCR = 0x00000000.
probably LSE ocillator isn't off.
thim my code :
#include 'stm32f10x.h'
#include 'stm32f10x_gpio.h'
#include 'stm32f10x_rcc.h'
int main(void){
PWR -> CR = 0x00000100;
RCC-> BDCR = 0x00000000.;
RCC_APB2PeriphClockCmd(RCC_APB2Perirh_GPIOC, ENABLE);
GPIO_InitTypeDef control;
control.GPIO_Pin = GPIO_Pin_14 | GPIO_Pin_15;
control.GPIO_Mode = GPIO_Mode_Out_PP;
control.GPIO_Speed = GPIO_Speed_2MHz;
GPIO_Init(GPIOC, &control);
while(1){
GPIO_SetBits(GPIOC, GPIO_Pin_15);
GPIO_SetBits(GPIOC, GPIO_Pin_14);
}
}
How can do this ?
Thanks,
Solved! Go to Solution.
2018-02-22 5:17 AM
I solved my problem. I made a mistake in one bit
BKP_RTCCR's register.
Thank you so much redwire and all friend.
2018-02-21 5:00 AM
I found only such limitations but have no experience with this:
When the backup domain is supplied by VDD (analog switch connected to VDD), the
following functions are available:• PC14 and PC15 can be used as either GPIO or LSE pins• PC13 can be used as GPIO, TAMPER pin, RTC Calibration Clock, RTC Alarm or second output (refer to Section 6: Backup registers (BKP))Note: Due to the fact that the switch only sinks a limited amount of current (3 mA), the use of GPIOs PC13 to PC15 in output mode is restricted: the speed has to be limited to 2 MHz with a maximum load of 30 pF and these IOs must not be used as a current source (e.g. to drive a LED).When the backup domain is supplied by VBAT (analog switch connected to VBAT because VDD is not present), the following functions are available:• PC14 and PC15 can be used as LSE pins only• PC13 can be used as TAMPER pin, RTC Alarm or Second output (refer toSection 6.4.2: RTC clock calibration register (BKP_RTCCR)).2018-02-21 5:25 AM
I saw this subjects in user manuel but don't choose. even sothank yo your helpfull Bogdan Golab.
2018-02-21 9:11 PM
I think your question has been answered but just in case you are looking for more info. There is no real issue with using PC14/15 as GPIO as long as you don't want to use the RTC with VBAT as stated above. My advice would be to use the CubeMX software to attempt this configuration and then optimize the code as required.
2018-02-22 5:17 AM
I solved my problem. I made a mistake in one bit
BKP_RTCCR's register.
Thank you so much redwire and all friend.
2020-05-12 11:28 PM
I have the same situation, what I'm doing wrong?
PWR_CR |= (uint32_t)PWR_CR_DBP;
RCC_BDCR = (uint32_t)0;
BKP_CR = (uint32_t)0;
BKP_RTCCR = (uint32_t)0;
BKP_CSR = (uint32_t)0;
RCC_BDCR |= (uint32_t)RCC_BDCR_BDRST;
gpio_set_mode(GPIOC, GPIO_MODE_OUTPUT_2_MHZ, GPIO_CNF_OUTPUT_PUSHPULL, GPIO14 | GPIO15);
GPIOC_BSRR |= GPIO14 | GPIO15;
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.