2014-12-18 12:25 PM
Hi I'm just playing around with the discovery board ST32F0
so I wrote a quick and dirty C app in CoIDE, started a ADC conversion etc and read in the on chip temp sensor. Thats all works fine ( or so it seems) even though I,m not calibrating it, nor compensating for the 3v versus 3v3 issue.What I get at rest on the board is decimal 1900-1927But strangely it counts lower when I put my finger on the chip and if I hit the chip with some freezer spray it counts higher ( like 20xx-21xx)weird ???any ideas thanksdave code below ( parts from a CoIDE demo)---------------&sharpinclude
<stdio.h>&sharpinclude
<stm32f0xx_gpio.h>&sharpinclude
<stm32f0xx_rcc.h>&sharpinclude
<stm32f0xx_adc.h>int
main(void
){
GPIO_InitTypeDefgpio;
ADC_InitTypeDef
ADC_InitStructure;RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOC,
ENABLE
);// Peripheral IO clock
RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1,
ENABLE
);// ADC Clock
GPIO_StructInit(&gpio);
gpio.
GPIO_Pin
= GPIO_Pin_9;// Green LED
gpio.
GPIO_Mode=
GPIO_Mode_OUT;
gpio.
GPIO_OType=
GPIO_OType_PP;
gpio.
GPIO_PuPd=
GPIO_PuPd_NOPULL;
gpio.
GPIO_Speed
= GPIO_Speed_50MHz;GPIO_Init(GPIOC, &gpio);
gpio.
GPIO_Pin
= GPIO_Pin_7;// Blue LED
GPIO_Init(GPIOC, &gpio);
/* Initialize ADC structure */ADC_StructInit(&ADC_InitStructure);
ADC_InitStructure.
ADC_ContinuousConvMode=
ENABLE;
ADC_InitStructure.
ADC_DataAlign
= ADC_DataAlign_Right;ADC_InitStructure.
ADC_Resolution
= ADC_Resolution_12b;ADC_InitStructure.
ADC_ScanDirection
= ADC_ScanDirection_Upward;ADC_InitStructure.
ADC_ExternalTrigConvEdge
= ADC_ExternalTrigConvEdge_None;ADC_Init(ADC1, &ADC_InitStructure);
ADC_ChannelConfig(ADC1,ADC_Channel_16,ADC_SampleTime_239_5Cycles);
ADC_TempSensorCmd(
ENABLE
);ADC_Cmd(ADC1,
ENABLE
);ADC_StartOfConversion(ADC1);
printf
(
''HelloDave
!\r\n'');
while(1)
{
static int
i;
static
int
led_state=0;uint16_t chip_temp;
for
(i=0; i<100000; ++i);GPIO_WriteBit(GPIOC, GPIO_Pin_9, led_state ?
Bit_SET
:Bit_RESET
);led_state = !led_state;
GPIO_WriteBit(GPIOC, GPIO_Pin_7, led_state ?
Bit_SET
:Bit_RESET
);
while
(ADC_GetFlagStatus(ADC1, ADC_FLAG_EOC) ==RESET
);// wait for conversion
chip_temp = ADC_GetConversionValue(ADC1);
printf
(
''ChipTemp
%d\r\n'', chip_temp);
}
}
#adc #discovery #stm32f0 #temp2014-12-18 1:20 PM
The on-chip sensor delivers a temperature proportional voltage. The on-chip parameter contain measured voltage at 30 and 110 degree and VDDA 3.3 V. With these values you have to calculate the temperature from the measured voltage.
2014-12-18 1:41 PM
''A thermistor is a passive device that changes its resistance with temperature. If the temperature-resistance characteristic is known, it can be used as a temperature sensor by measuring the resistance, or more precisely, the voltage across it. Thermistors are classified in to two types: NTC (negative temperature coefficient) and PTC (positive temperature coefficient). A NTC thermistor decreases its resistance while the temperature rises, and a PTC does the opposite.
http://embedded-lab.com/blog/?p=1019
Still weird? Aren't the set points stored in System Memory, so as to define the actual slope?2014-12-18 2:17 PM
See Section 12.9 in the reference manual. The formula is:
Temperature (in °C) = {(V25 – VSENSE) / Avg_Slope} + 25 As VSENSE decreases, calculated Temperature increases. The confusing part is that the formula assumes an unsigned slope. Cheers, HalWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.