STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F303: ADC interleave mode overrun

Posted on December 19, 2014 at 16:30Hello,With  the STM32F303RC, I use ADC12 in interleave mode with 2 DMA to reach a 10.2 Ms sampling rate.The ADC acquisition is trigged internally by TIM2 every 1ms, I read 1500 samples during ~100µs .That's was wo...

Stm32f103 Memory Jumping with parameters

Posted on December 17, 2014 at 13:46Hello, I'm working with the STM32f103RB and I'm trying to jump to a section of flash where I will begin executing another program there My code should look like this (variable ApplicationAddress is 0x08008000) :  ...

cnhx27 by Associate III
  • 3630 Views
  • 9 replies
  • 0 kudos

TIM SYNCHRONIZED

Posted on December 18, 2014 at 22:56The original post was too long to process during our migration. Please click on the attachment to read the original post.

franck2 by Associate II
  • 1107 Views
  • 1 replies
  • 0 kudos

STM32 isochronous transfer

Posted on December 19, 2014 at 08:33 how to transfer 512 bytes? Send_DATA ((unsigned char *)trBuffer, 512); void Send_DATA(uint8_t* ptrBuffer, uint16_t Send_length) { if (GetENDPOINT(ENDP1) & EP_DTOG_RX) // NOT TX ie SW_BUF { U...

FatFS problem with SDIO on stm32f103vet6

Posted on December 18, 2014 at 16:23Hi guys, I'm trying to use an SD card with the aforementioned chip on the Primer2. I started from a working project but when ported to my application, it simply doesn't work. Anyone can help?In detail, I've ported...

angeletti by Associate II
  • 2974 Views
  • 8 replies
  • 0 kudos

STM32F072 temp sensor counts wrong way !!

Posted on December 18, 2014 at 21:25Hi I'm just playing around with the discovery board ST32F0so I wrote a quick and dirty C app in CoIDE, started a ADC conversion etc and read in the on chip temp sensor. Thats all works fine ( or so it seems) even ...

STM32F407 USART3 DMA Transmit problem

Posted on December 18, 2014 at 13:32 Hello Everyone I am tryint to send data through usart3 by dma ; I can send data without DMA but when configure to use the DMA I could not send ; Could you guide me to check my mistakes ; the code ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.