2016-11-10 4:21 AM
Hi,
I am STM32f030C8T6 MC along with L80 GPS in USART1 and Quectel Modem M35 in USART2 for live tracking purpose.The coding is done using COOCOX CO IDE. All Idone is I had successfully taken Latitude and Longitude from GPS and pushed to web-server using GPRS of the modem. upto this i had to prblm, the only problem is i cant able to read reply returned by modem to controller even using Interrupt . Here is the sample i have been trying for about two days,
#include <
stdint.h
>
#include <
stdio.h
>
#include <
stdio_ext.h
>
#include <
stm32f0xx_gpio.h
>
#include <
stm32f0xx_rcc.h
>
#include <
stm32f0xx_usart.h
>
#include <
semihosting.h
>
#include <
stm32f0xx_misc.h
>
#include <
string.h
>
#include <
math.h
>
char temp_buff[200]={'\0'};//,temp_buff1[200]={'\0'};
short irq_bit=0,okflag=0,data_received_bit=0,RMCGot=0,GGAGot=0,flag=0;
void USART1_IRQ(void)
{
char ch = 0;
static uint8_t SentenceBegin = 0, SentenceCnt = 0;
//static char TmpBuf[200];
if( USART_GetFlagStatus(USART1,USART_FLAG_RXNE)== SET)
{
USART_ClearFlag(USART1,USART_FLAG_RXNE);
ch=USART_ReceiveData(USART1);
if(ch=='$')
{
SentenceBegin=1;
SentenceCnt=0;
}
if(ch == '\n' && SentenceBegin)
{
printf(''%s \n'',temp_buff);
if(temp_buff[3]=='R' && temp_buff[4]=='M' && temp_buff[5]=='C')
{
RMCGot=1;
//gps_data(30,0);
//GGAGot=0;
}
if(temp_buff[3]=='G' && temp_buff[4]=='S' && temp_buff[5]=='V')
{
//RMCGot=0;
GGAGot=1;
}
SentenceBegin = 0;
flag=1;
}
if(SentenceBegin)
{
temp_buff[SentenceCnt] = ch;
SentenceCnt++;
}
}
}
void USART2_IRQ(void)
{
char c = 0;
static short SentenceB1 = 0, SentenceC1 = 0;
short size=0;
static char temp_buff1[200];
if( USART_GetFlagStatus(USART2,USART_FLAG_RXNE)== SET)
{
USART_ClearFlag(USART2,USART_FLAG_RXNE);
c=USART_ReceiveData(USART2);
if((c!='\n') && (c!='\0') && (SentenceB1==0))
{
SentenceB1=1;
SentenceC1=0;
irq_bit=1;
}
if(c == '\n' && SentenceB1)
{
temp_buff1[SentenceC1]='\0';
size=SentenceC1;
printf(''USART2:%s %d\n'',temp_buff1,SentenceC1);
if(temp_buff1[0]=='O' && temp_buff1[1]=='K')
{
okflag=1;
}
if((temp_buff1[0]=='d') && (temp_buff1[1]=='a') && (temp_buff1[2]=='t') && (temp_buff1[3]=='a') && (temp_buff1[4]==0x20) && (temp_buff1[5]=='r') && (temp_buff1[6]=='e') && (temp_buff1[7]=='c') && (temp_buff1[8]=='i') && (temp_buff1[9]='e') && (temp_buff1[10]=='v') && (temp_buff1[11]=='e') && (temp_buff1[12]=='d'))
{
data_received_bit=1;
}
{
for(int j=0;j<(size-1);j++)
{
temp_buff1[j]=0;
}
}
SentenceB1 = 0;
SentenceC1 = 0;
}
if(SentenceB1 && c!='\0')
{
temp_buff1[SentenceC1] = c;
SentenceC1++;
}
}
}
int main(void)
{
short j=0,k=0,first_flag=0;
uint8_t reg=0;
uint64_t i=0;
// short number[10]={0,0,0,0,0,0,0,0,0};
USART_InitTypeDef USART_InitStructure;
GPIO_InitTypeDef GPIO_InitStructure;
NVIC_InitTypeDef N;
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB, ENABLE); // Enable GPIO A bank clock
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOC, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1,ENABLE); // Enable USART1 clock
RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2,ENABLE); // Enable USART1 clock
/* Configure Alternate Function pin muxing fabric to escape USART1 Rx and Tx */
GPIO_PinAFConfig(GPIOA, GPIO_PinSource10, GPIO_AF_1);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource2, GPIO_AF_1);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource3, GPIO_AF_1);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_13; // Green LED
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_Level_1;
GPIO_Init(GPIOC, &GPIO_InitStructure);
/* Configure USART1 pins: Rx and Tx */
// GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10 ;
// GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
// GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
// GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
// GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
// GPIO_Init(GPIOA, &GPIO_InitStructure);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_Init(GPIOA, &GPIO_InitStructure);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_3 |GPIO_Pin_10 ;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init(GPIOA, &GPIO_InitStructure);
/* Enable USART1 IRQ */
/* Configure USART1 settings */
USART_InitStructure.USART_BaudRate = 9600;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Rx ;
USART_Init(USART1, &USART_InitStructure);
USART_InitStructure.USART_BaudRate = 9600;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
USART_Init(USART2, &USART_InitStructure);
USART_OverrunDetectionConfig(USART1, USART_OVRDetection_Disable);
USART_OverrunDetectionConfig(USART2, USART_OVRDetection_Disable);
USART_Cmd(USART1,ENABLE); // Enable USART1
USART_Cmd(USART2,ENABLE);
// N.NVIC_IRQChannel = USART2_IRQn;
// N.NVIC_IRQChannelCmd = ENABLE;
// N.NVIC_IRQChannelPriority = 0;
// NVIC_Init(&N);
// NVIC_EnableIRQ(USART2_IRQn);
// USART_ITConfig(USART2,USART_IT_RXNE,ENABLE);
// N.NVIC_IRQChannel = USART1_IRQn;
// N.NVIC_IRQChannelCmd = ENABLE;
// N.NVIC_IRQChannelPriority = 1;
// NVIC_Init(&N);
// NVIC_EnableIRQ(USART1_IRQn);
// USART_ITConfig(USART1,USART_IT_RXNE,ENABLE);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_14; // Green LED
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_Level_1;
GPIO_Init(GPIOB, & GPIO_InitStructure);
GPIO_WriteBit(GPIOB, GPIO_Pin_14,Bit_SET);
for (i=0; i<2500000;i++);
GPIO_WriteBit(GPIOB, GPIO_Pin_14, Bit_RESET);
USART2_IRQ();
while(1)
{
USART1_IRQ();
USART2_IRQ();
}
in the above i didnt used interrupt for USART2 , but i tried that one too. one more thing the Usart 1 works fine with Interrupt and without interrupt. the only prblm is Usart 2. When the modem is powered it reply with Call ready and Cpin ready, i cant able to read these things also.
#- #stm32f0 #quectel-m352016-11-10 4:56 AM
I tend to prefer using ring buffers.
So what exactly is the code receiving? It is hard to look at the code alone, without some context. Do you get the data you expect from the modem, and your code just doesn't react to it in the manner you expect? Should you put some bounds checking on the buffers? Your code looks for GSV not GGA You don't need to clear RXNE, reading the data register will do this automatically.2016-11-10 9:36 PM
#include <
stdint.h
>
#include <
stdio.h
>
#include <
stdio_ext.h
>
#include <
stm32f0xx_gpio.h
>
#include <
stm32f0xx_rcc.h
>
#include <
stm32f0xx_usart.h
>
#include <
semihosting.h
>
#include <
stm32f0xx_misc.h
>
#include <
string.h
>
#include <
math.h
>
char temp_buff[200]={'\0'},temp_buff1[300]={'\0'};
int main(void)
{
short j=0,k=0,first_flag=0;
uint8_t reg=0;
uint64_t i=0;
// short number[10]={0,0,0,0,0,0,0,0,0};
USART_InitTypeDef USART_InitStructure;
GPIO_InitTypeDef GPIO_InitStructure;
NVIC_InitTypeDef N;
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB, ENABLE); // Enable GPIO A bank clock
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOC, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1,ENABLE); // Enable USART1 clock
RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2,ENABLE); // Enable USART1 clock
/* Configure Alternate Function pin muxing fabric to escape USART1 Rx and Tx */
GPIO_PinAFConfig(GPIOA, GPIO_PinSource10, GPIO_AF_1);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource2, GPIO_AF_1);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource3, GPIO_AF_1);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_13; // Green LED
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_Level_1;
GPIO_Init(GPIOC, &GPIO_InitStructure);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_Init(GPIOA, &GPIO_InitStructure);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_3 |GPIO_Pin_10 ;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init(GPIOA, &GPIO_InitStructure);
/* Enable USART1 IRQ */
/* Configure USART1 settings */
USART_InitStructure.USART_BaudRate = 9600;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Rx ;
USART_Init(USART1, &USART_InitStructure);
USART_InitStructure.USART_BaudRate = 9600;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
USART_Init(USART2, &USART_InitStructure);
USART_OverrunDetectionConfig(USART1, USART_OVRDetection_Disable);
USART_OverrunDetectionConfig(USART2, USART_OVRDetection_Disable);
USART_Cmd(USART1,ENABLE); // Enable USART1
USART_Cmd(USART2,ENABLE);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_14; // POWER KEY FOR MODEM
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_Level_1;
GPIO_Init(GPIOB, & GPIO_InitStructure);
GPIO_WriteBit(GPIOB, GPIO_Pin_14,Bit_SET);
for (i=0; i<2500000;i++);
GPIO_WriteBit(GPIOB, GPIO_Pin_14, Bit_RESET);
while(1)
{
while( USART_GetFlagStatus(USART2,USART_FLAG_RXNE)== SET)
{
// USART_ClearFlag(USART2,USART_FLAG_RXNE);
char c= (char)USART_ReceiveData(USART2);
printf(''u :%c
'',c);
c='\0';
}
}
}
2016-11-10 10:54 PM
Hi Clive1,
I forgot to tell you the connection setup, I had connected modem RX to PC via FTDi, and Modem TX to Rx of Controller. for initial testing purpose. thus i giving AT from PC and receiving reply in Micro-controllerWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.