STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

The example of receiving ethrnet frames

Posted on November 08, 2016 at 09:43Hi!I am the beginner in ethernet on STM32F407.I connected STM32F407 to LAN8720, LAN8720 connected through ethernet cable to PC.   I set IP-address 192.168.0.10 (255.255.255.0) for the PC and on the PC I did ping 1...

Stop Mode and Spi Peripheral Behaviour

Posted on November 11, 2016 at 11:50Hello Everyone,In our application , Radio is connected to  stm32f4 series MCU via SPI and radio Irq line connected to one of the Exti line of mcu. Before putting into the stop mode, radio has been configured . Upo...

STM32F746 Discovery transfer data via Ethernet

Posted on November 10, 2016 at 19:39Greetings!We are having a project in our class where we are using a  STM32F746 touch system. We have programmed a code where we store some data on a file. I am wondering if anyone could guide me to how to transfer...

Problem with initialization ADC2 STM32L476RET in HAL

Posted on November 10, 2016 at 15:10Good day! I use microcontroller stm32l476ret. In CubeMX create desired configuration and  create  project for Keil v.5. The Keil everything compiles without errors. Pour the code into the microcontroller. The mic...

STM32F030C8T6 with quectel M35 in USART2 Receiving Problem

Posted on November 10, 2016 at 13:21 Hi, I am STM32f030C8T6 MC along with L80 GPS in USART1 and Quectel Modem M35 in USART2 for live tracking purpose.The coding is done using COOCOX CO IDE. All Idone is I had successfully taken Latitu...

raj11 by Associate II
  • 1913 Views
  • 3 replies
  • 0 kudos

STM32F746V

Posted on November 09, 2016 at 14:40Can anybody point me at a document for the the pin configuration for the 'F746 100 pin package. I can't find LCD_B1 on the data sheet or in the reference manual. I assume there is something else as the 'how to con...

nigelh by Associate II
  • 1633 Views
  • 4 replies
  • 0 kudos

STM32F4+SD+Interrupt Problem

Posted on November 10, 2016 at 11:59Hi all, I'm trying to write a code of a data logger with the following characteristics: A string is captured using interruptions by a uart at 921600 bauds: The information is stored byte by byte, and the whole s...

vicfer89 by Associate II
  • 2119 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.